LPC8N04 Wakeup from Deep-Power-Down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC8N04 Wakeup from Deep-Power-Down

1,341 Views
kenchill
Contributor III

LPC8N04 Wakeup from Deep-Power-Down.

We have a project that requires the LPC8N04 to wakeup from DPD by NFC, RTC or WAKEUP pin, the problem is detecting the source of wakeup - as the LPC8N04 cannot be debugged in DPD we are toggling i/o pins to detect states.

1) We are finding that it takes 6ms or so before any NFC status flags can be used (apart from the PSWNFC bit in the PSTAT register).

2) When woken by either NFC or WAKEUP pin the 'RTC Timer Event' flag gets set in the PSTAT register - this flag doesn't get set if the RTC woke the device.

3) If the RTC wakes the device the 'LDO Enabled' flag gets set in the PSTAT register.

Are we missing something? Or is this how the LPC8N04 functions? If it is how the LPC8N04 functions is it reliable and safe to use these flags?

I hope someone can help

Thanks in advance

Ken...

0 Kudos
Reply
1 Reply

1,228 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

The NFC status flags should wait to the chip get ready, it should depend on detailed application initial process.

For wake up flag of different wake up source, Could you check DPDFLAG in the PCON register whether asserted in your testing code? It need be asserted to get DPDEXIT flag work. 

BR,

Ivan.

0 Kudos
Reply