Is there a hardware setting (wiring) for MFRC630 to keep it always on regardless of the host (or can I simply delete the host?)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a hardware setting (wiring) for MFRC630 to keep it always on regardless of the host (or can I simply delete the host?)?

ソリューションへジャンプ
1,506件の閲覧回数
ivanqi
Contributor I

Is there a hardware setting (wiring) for MFRC630 to keep it always on regardless of the host (or can I simply delete the host?)? The goal is to use it simply as a 13.56MHz RF power generator...

タグ(3)
1 解決策
1,427件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Ivan,

    below is advice for you :

(1) MCU must be used.

Because you need to configure MFRC630 via software.

(2) Make if always on

you don't need to use additional hardware, if you don't set Standby or Power down mode, it will be always on.


Have a great day,
TIC  Weidong sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,428件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Ivan,

    below is advice for you :

(1) MCU must be used.

Because you need to configure MFRC630 via software.

(2) Make if always on

you don't need to use additional hardware, if you don't set Standby or Power down mode, it will be always on.


Have a great day,
TIC  Weidong sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,427件の閲覧回数
ivanqi
Contributor I

Well answered. Thank you sir :smileyhappy:

0 件の賞賛
返信