Hello everyone,
I'm working on a little project using:
The idea is to use the MFRC522 solely to wakeup the BLE module.
Reading the BLE module documentation, it says the peripheral features an NFC-A listen mode operation, at 13,56MHz and 106 kbps bit rate, called SENSE mode. As I don't want to exchange data with the module, as I understand, all I need to do is to expose the module to a 13,56MHz NFC field, and the module will wakeup. That is working, but at a very short range.
I want to know how can I maximize the range. How can I increase the "Output Power" for the MFRC522, specifically?
Thanks.
Hello,
As this devices does not have DPC , it is not possible to achieve your request through software. The way to increase the signal strength would be through the antenna design, nonetheless, as you are using a module from a third party the passive elements of the antenna are already defined in your board.
Sorry for the inconveniences this might cause you.
Regards,
Estephania