Custom board USB - PN7462

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom board USB - PN7462

ソリューションへジャンプ
1,258件の閲覧回数
benten
Contributor II

Hi All,

We develop custom board with PN7462 with USB support.  We created the same two PCBs. And we wrote to flash phExCcid app.

One of them works. One of them has a problem with connection USB because OS said "Unknown USB Device (Device Descriptor Request Failed)". We see that hwUSB_Init retuns LPC_OK. And we see that HIF_IRQHandler is called.

We excluded that is soldering responsible.

Do you have any ideas what we should do/check?

Thanks,

Kamil

0 件の賞賛
返信
1 解決策
1,123件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

This sounds like a hardware problem of the design if one board works and the other does not. Please check voltage levels on VDD and TVDD to make sure that the board is properly powered and check that correct components are on their place.

It will be helpful to refer to PN7462 eval board design files:

Layout: https://www.nxp.com/downloads/en/schematics/DF4823.PDF 

Schematics: https://www.nxp.com/downloads/en/schematics/DF4824.PDF 

Regards,

Ivan.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,124件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

This sounds like a hardware problem of the design if one board works and the other does not. Please check voltage levels on VDD and TVDD to make sure that the board is properly powered and check that correct components are on their place.

It will be helpful to refer to PN7462 eval board design files:

Layout: https://www.nxp.com/downloads/en/schematics/DF4823.PDF 

Schematics: https://www.nxp.com/downloads/en/schematics/DF4824.PDF 

Regards,

Ivan.

0 件の賞賛
返信
1,123件の閲覧回数
benten
Contributor II

We changed IC -> its helps. Thank you.

0 件の賞賛
返信