CLRC663 ISO15693 Anticollision

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663 ISO15693 Anticollision

1,557 Views
liurui
Contributor I

Hello,

Can you show me the code about ISO15693 Anticollision.

Thanks

0 Kudos
Reply
2 Replies

1,539 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @liurui 

Unfortunately, we do not have the source code for ISO 15693 Anti-collision, but have source code based on ISO 14443. If you need and download SW6693 which is open-source code.

To update this case, you may reply by email.
To provide confidential information or attachments, you may add that online.

Please login to our NXP technical support portal:
https://support.nxp.com/s/case/5002p00002qXWOOAA4

The portal allows access to the full details of the case, including the previous communication.

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

Best regards,
Kelly
Technical Support
NXP Semiconductor

0 Kudos
Reply

1,509 Views
liurui
Contributor I

Thanks.

0 Kudos
Reply