PMSM FOC control with position sensor (encoder)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PMSM FOC control with position sensor (encoder)

跳至解决方案
4,418 次查看
peterkostadinov
Contributor III

Hi All,

I need example project with PMSM FOC control, but with position sensor (encoder), instead of available examples, which are SENSORLESS.

Best Regards,

Peter

0 项奖励
回复
1 解答
4,037 次查看
philip_drake
NXP Employee
NXP Employee

Please see this Application Note: 

    • AN12374

There is an encoder project in the software package as well as a hall effect start-up FOC software project.

Regards,

Philip

在原帖中查看解决方案

4 回复数
4,037 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Peter,

Besides the FRDM-KV31 solution for PMSM FOC control based on encoder sensor as Philip pointed out, this is the DSC solution. Pls download "PMSM_FOC_ENCODER_MC56F84789_TWR_DEMO" from the following link:

PMSM FOC Industrial Drives Reference Design | NXP 

Hope it can help you

BR

XiangJun Rong

4,037 次查看
peterkostadinov
Contributor III

Thank you very much for your support!

Best Regards,

Peter

0 项奖励
回复
4,038 次查看
philip_drake
NXP Employee
NXP Employee

Please see this Application Note: 

    • AN12374

There is an encoder project in the software package as well as a hall effect start-up FOC software project.

Regards,

Philip

4,037 次查看
peterkostadinov
Contributor III

Thank you very much for your support!

Best Regards,

Peter

0 项奖励
回复