Freemaster with KV31: Can not detect Board information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster with KV31: Can not detect Board information

Jump to solution
859 Views
pbgemann001
Contributor III

Hello,

my setup is a KV31F120M and the Motor Control Toolbox on Matlab2019a / Windows. I have successfully compiled and downloaded a simple LED example (attached). Now I want to establish a connection to Freemaster.

I did the following:

- Add the Freemaster Data Recorder Block to the Model

- Freemaster Config -> UART1 / Baudrate: 9600

- Build

- Freemaster -> Options -> COM7 (OpenSDA) / Speed: 9600

- Start Communication leads to the ERROR: "Can not detect board Information! Communication will be paused."

Any Ideas on how to solve this issue?

Tags (2)
0 Kudos
1 Solution
657 Views
pbgemann001
Contributor III

Found the solution: Should be UART0 Pin: PTB16 and PTB17

View solution in original post

1 Reply
658 Views
pbgemann001
Contributor III

Found the solution: Should be UART0 Pin: PTB16 and PTB17