TWR-K60N512 + IAR + MQX example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K60N512 + IAR + MQX example

ソリューションへジャンプ
801件の閲覧回数
sebasira
Senior Contributor I

Hello to you all!!

I'd like to get started with K60 MCU and MQX. I can't seem to find any code example for MQX and TWR-K60N512...I' using IAR v6.3

I've installed:

- MQX 3.8

- TWRK60N512QSDLAB.exe

Thanks!

タグ(3)
0 件の賞賛
返信
1 解決策
560件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hello, the code examples are in mqx/examples, usb/device/examples, usb/host/examples, rtcs/examples, mfs/examples folders for MQX 3.8 installation.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
561件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hello, the code examples are in mqx/examples, usb/device/examples, usb/host/examples, rtcs/examples, mfs/examples folders for MQX 3.8 installation.

0 件の賞賛
返信
560件の閲覧回数
sebasira
Senior Contributor I

Hi Juraj, thanks for your reply!

I've seen them, but I was use to have an IDE Workspace file that I will open with IAR... now I discover, the "Add Existing Project" option.

Thanks!!!

0 件の賞賛
返信