PHY KSZ8051MLL Integration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PHY KSZ8051MLL Integration

1,628 Views
payyans4u
Contributor I

Hi,

 

I am currently working on MCF52259 with CW 7.2 ...i am using a PHY KSZ8051MLL...The demo kit that i have has  a Micrel 8041 NL PHY.....Do anyone here have a working knowledge of KSZ8051 MLL...or atleast if sumbody could tell me the difference between the two would be of great help....Thanks in advance

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,275 Views
Weining
Contributor III

I am using the same things. the driver for the demo board (for 8041) works well for KSZ8051 on my board. I had talked to the Micrel applcation engineer, he mentioned that Micrel does not change any register addresses from 8041 to 8051.

 

the main difference between 8041 and 8051 might be the hardware,  you could check Micrel application note AN-143.