Hi, I´m using a mqx project on a custom board with a MK53N512CMD10 and an external cristal of 8MHz. I try to use the proccesor expert to configure the external cristal, and got stuck on this line of code at dispatch.S file:
ASM_LABEL(no_one_to_run)
/ woohoo, idle task must be enabled, this point cannot be reachable, you have serious problem /
b .
¿does the K53N512CMD10 with MQX support an external cristal of 8MHz?
¿How do i configure MQX to work with the external cristal of 8MHz?
¿How do i link my MXQ proyect with a bsp clon?
I'll be thankful for your help
Regards
Alberto
解決済! 解決策の投稿を見る。
Hello Alberto,
I have reviewed this issue and this may helps.
The TWR-K53N512 BSP has been created for the TWR-K53N512, Rev.C schematics (SCH-26994), Rev.X3 BOM
(700-26694). This TWR-K53N512 board is populated by PK53N512CMD100. The BSP does not work for TWRK53N512
boards populated by MK53DN512CMD10 with the 4N22D mask set. A workaround is to use the
twrk60d100m BSP for this kind of TWR-K53N512 board.
I think this is the issue. Could you please try again cloning the wtrk60d100m BSP instead the twrk53?
Please let me know if this helps.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Alberto,
I have reviewed this issue and this may helps.
The TWR-K53N512 BSP has been created for the TWR-K53N512, Rev.C schematics (SCH-26994), Rev.X3 BOM
(700-26694). This TWR-K53N512 board is populated by PK53N512CMD100. The BSP does not work for TWRK53N512
boards populated by MK53DN512CMD10 with the 4N22D mask set. A workaround is to use the
twrk60d100m BSP for this kind of TWR-K53N512 board.
I think this is the issue. Could you please try again cloning the wtrk60d100m BSP instead the twrk53?
Please let me know if this helps.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------