Hello at present, I'm trying to work with the new develoment tool "Kinetis Design Studio". I want to develop an aplication with MQX in the FRDM-K64F.
I've tried to create a project MQX in KDS for differents ways:
*Create a project in Codewarrior 10.6 and import to KDS.(not compile)
*Create a project in KDS with/without Process Expert and KSDK.
*Create a simple project with Process Expert and KSDK, and include the component MQX and MQX task in my project.
Of the last two forms, I get to compile without errors, but i can't debug. Show the error "Can not read register XX (XX) while CPU is running".
How can i work with KDS and MQX? How can i create a MQX project?
Thanks for the help.
已解决! 转到解答。
Hello,
With IAR and Keil we don't have any wizard, copy&paste the folder Project use to work. But some paths need to be modified.
For KDS would have to do the same.
Perhaps there is an easier path, but this one works for me.
Best Regards,
Luis
Hello,
With IAR and Keil we don't have any wizard, copy&paste the folder Project use to work. But some paths need to be modified.
For KDS would have to do the same.
Perhaps there is an easier path, but this one works for me.
Best Regards,
Luis