CDC over MQX 4.1 in K70F120M series.Issue : CDC is not working: Enumeration does not happen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CDC over MQX 4.1 in K70F120M series.Issue : CDC is not working: Enumeration does not happen

646 Views
HarshGoel
Contributor I

We are using K70F120M series .

OS: MQX 4.1

Requirements : CDC over MQX 4.1 in  K70F120M series.

Issue : CDC is not working: Enumeration does not happen

Observation : Freescale_BM_USB_Stack_v5.0 is released and we can configure to work with MQX or non-OS.

Query : Does is solves the issue of CDC if yes then in which what MQX or bare- metal.

Tags (1)
0 Kudos
Reply
1 Reply

387 Views
Carlos_Musich
NXP Employee
NXP Employee

Hello Harsh,

I ran the MQX4,1 Virtual Com Port example using K70 and I had no problems.

Please see the document in link below showing step by step how tu run the example:

https://community.freescale.com/docs/DOC-101404

Best regards,

Carlos

0 Kudos
Reply