Hi,
I am using the nxp5748G board and I checked the lwip_5748g example, In which Board works as a server and PC works as a client.
I want to make the board work in client mode, Is there any example or information which I can refer?
Hi,
I'm afraid we do not have more examples. There are only two examples in the SDK:
c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5748G\demo_apps\lwip\
c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5748G\demo_apps\usb_cdc_lwip\
Because lwip is not owned by us, I would recommend:
https://lwip.fandom.com/wiki/Further_lwIP_support
Regards,
Lukas