mpc5748G board works as a client

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc5748G board works as a client

491 Views
jiteshka
Contributor I

Hi,

I am using the nxp5748G board and I checked the lwip_5748g example, In which Board works as a server and PC works as a client.

I want to make the board work in client mode, Is there any example or information which I can refer?

0 Kudos
Reply
1 Reply

482 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm afraid we do not have more examples. There are only two examples in the SDK:

c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5748G\demo_apps\lwip\

c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5748G\demo_apps\usb_cdc_lwip\

Because lwip is not owned by us, I would recommend:

https://lwip.fandom.com/wiki/Further_lwIP_support

Regards,

Lukas

 

0 Kudos
Reply