led

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,633件の閲覧回数
smallyang
Contributor III

亲们我请教下,例程led我们想改两个引脚。是只用改这个数字嘛?  其他的我们需要改动嘛 ?  例子用的这个113,手册上和我们用87和88看起来是差不多的。

Dear, let me ask you, routine led we want to change two pins. Are we just gonna change this number? Do we need to change anything else? The example uses 113, which in the manual looks pretty much the same as we used 87 and 88.

smallyang_0-1712712737441.jpeg

 

smallyang_1-1712712746750.png

 

smallyang_2-1712712757534.png

smallyang_3-1712712778747.png

smallyang_4-1712712819490.jpeg

 

smallyang_5-1712712834870.png

 

 

 

0 件の賞賛
返信
1 解決策
1,581件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please see the reference manual for configuration of internal flash boot:

petervlna_0-1712828189701.png

Best regards,

Peter

 

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
1,612件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am confused from your post.

Which microcontroller you are speaking about? Do you have a NXP EVB or your own board?

What you want to achieve? You want to change output state of specific GPIO pins? Which ones?

Best regards,

Peter

0 件の賞賛
返信
1,597件の閲覧回数
smallyang
Contributor III

您好,  我有个新的问题。   我想问下电路板这些引脚怎么设置才能用同调试器从jtag口下载调试呢?

Hello, I have a new question. I would like to ask how to set these pins of the circuit board to download debugging from the jtag port with the debugger?

smallyang_0-1712807363000.png

smallyang_1-1712807531058.png

 

 

 

0 件の賞賛
返信
1,582件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please see the reference manual for configuration of internal flash boot:

petervlna_0-1712828189701.png

Best regards,

Peter

 

0 件の賞賛
返信
1,565件の閲覧回数
smallyang
Contributor III

smallyang_0-1712884027748.png

 

externa. watchdog    Hello, How to remove watchdog?

 

0 件の賞賛
返信
1,577件の閲覧回数
smallyang
Contributor III

TEST = 0:

smallyang_1-1712829047075.png

 

TEST = 1  :

smallyang_0-1712829022681.png

What about the other pins?

0 件の賞賛
返信
1,578件の閲覧回数
smallyang
Contributor III

PLLCFG0 PLLCFG1  WKPCFG  TEST EVTI

0 件の賞賛
返信
1,579件の閲覧回数
smallyang
Contributor III

好的谢谢您,我用RAM也是这样配置吗 ,其他引脚呢

Ok, thank you. Do I use RAM in the same way? What about the other pins?

smallyang_0-1712828421600.png

 

smallyang_1-1712828446583.png

 

0 件の賞賛
返信
1,611件の閲覧回数
smallyang
Contributor III

您好,我们想把led Example_MPC5554EVB-PinToggleStationery-v0_2-CW210的gpio113改成gpio87

 

Hello, we want to change gpio113 of led Example_MPC5554EVB-PinToggleStationery- V02-CW210 to gpio87

0 件の賞賛
返信