[elxr] (error #21) cannot find library -lmulti

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[elxr] (error #21) cannot find library -lmulti

跳至解决方案
1,878 次查看
tmduybk
Contributor II

Hi,

I download Example MPC5748G Flash RW GHS614.

But when I using command line "gbuild -top MPC5748G-Flash_RW-GHS614.gpj", cmd show Error:

[elxr] (error #21) cannot find library -lmulti

I attach image of an error. Thank you !

0 项奖励
回复
1 解答
1,852 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

not sure what's the root cause here but the example is very simple piece of code, so you can only copy the code from main.c and add it to your project (to any IDE). No other files are needed or modified.

Regards,

Lukas

 

在原帖中查看解决方案

1 回复
1,853 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

not sure what's the root cause here but the example is very simple piece of code, so you can only copy the code from main.c and add it to your project (to any IDE). No other files are needed or modified.

Regards,

Lukas