Hello,
It seems not possible to create a etpu2 CW function set all motor control function on it (PMSM + FOC + AS + Resolver+ QD)
I get this error :
"
Now it is corrected and it seems it is working fine.
Thanks it is working now.
A comment about this, the other motor control eTPU function (for exemple PWMM) seem also different between eTPU and eTPU2 (different size)
I have actually an issue where the PWMM eTPU1 function works and the eTPU2 version doesnt work (see https://community.nxp.com/thread/498000)
Thanks again,
Daniel
Hi, yesterday functions from motor control set has been updated. Please check it again and let me know if the issue disappear.
Hi, it is known to me. I have already discussed with eTPU expert.
The problem is (as it is currently placed in the CodeWarrior eTPU Function Selector) QD function is only written for eTPU2 and the rest of motor control library is only written for eTPU and this way it can currently be downloaded as two function sets. Otherwise the compiler reports mentioned error.
It has been reported and it should be corrected very early.