S32R274 - PLL registers & configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32R274 - PLL registers & configuration

979件の閲覧回数
riccardo_ertolu
Contributor II

Hello everybody,

I'm working on S32R274 and I want to set the PLL with the following setup:

  • Internal RC oscillator as the source for PLL0
  • The PLL0 as the source for system clock
  • PLL0 @ 160MHz setting prediv=2, mfd=40; rfd=2

To do that I should properly set the following registers:

  • MC_CGM_AC3_SC
  • PLLDIG_PLL0DV
  • ME_DRUN_MC

And then check ME_GS to see if the setup was activated.

My questions are:

  1. What is the base address of the PLLDIG module?
  2. Is my setup correct?

Thanks in advance for the help!

ラベル(1)
タグ(2)
2 返答(返信)

884件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1. the memory map is given within Excel sheet attached to the Reference Manual.
From this you can find base address of MC_CGM as 0xFFFB0000 and FM_PLL (PLLDIG) offset addres w.r.t MC_CGM as 0x100. Thus base address of PLLDIG will be 0xFFFB0100.

2. for a clock setting code you can refer to some demos posted here :https://community.nxp.com/docs/DOC-329623#S32R274

It does not set to run PLL from IRC, but you can do little modification if needed.

BR, Petr

884件の閲覧回数
riccardo_ertolu
Contributor II

Hello Petr,

thanks a lot for your reply, I just found that into the excel file.
It's a bit tricky because for similar devices you use a different style to define the address of the PLLDIG.

One last question: should I also set the FT_DIS bit to 1 for all the RAM controllers when setting the frequency so high, like 160MHz?

Thanks

0 件の賞賛
返信