S32R274 - PLL registers & configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R274 - PLL registers & configuration

755 Views
riccardo_ertolu
Contributor II

Hello everybody,

I'm working on S32R274 and I want to set the PLL with the following setup:

  • Internal RC oscillator as the source for PLL0
  • The PLL0 as the source for system clock
  • PLL0 @ 160MHz setting prediv=2, mfd=40; rfd=2

To do that I should properly set the following registers:

  • MC_CGM_AC3_SC
  • PLLDIG_PLL0DV
  • ME_DRUN_MC

And then check ME_GS to see if the setup was activated.

My questions are:

  1. What is the base address of the PLLDIG module?
  2. Is my setup correct?

Thanks in advance for the help!

Labels (1)
Tags (2)
2 Replies

660 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1. the memory map is given within Excel sheet attached to the Reference Manual.
From this you can find base address of MC_CGM as 0xFFFB0000 and FM_PLL (PLLDIG) offset addres w.r.t MC_CGM as 0x100. Thus base address of PLLDIG will be 0xFFFB0100.

2. for a clock setting code you can refer to some demos posted here :https://community.nxp.com/docs/DOC-329623#S32R274

It does not set to run PLL from IRC, but you can do little modification if needed.

BR, Petr

660 Views
riccardo_ertolu
Contributor II

Hello Petr,

thanks a lot for your reply, I just found that into the excel file.
It's a bit tricky because for similar devices you use a different style to define the address of the PLLDIG.

One last question: should I also set the FT_DIS bit to 1 for all the RAM controllers when setting the frequency so high, like 160MHz?

Thanks

0 Kudos