Quadrature

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Quadrature

4,271 次查看
zhang_ke_dong
Contributor I

When the eTimer module of MPC5744P decodes ABI orthogonally, there is a problem in reading the CNTR register value at low motor speed?

MPC5744P chip SDK3.0.3 How to set the comparison value to zero after CNTR reaches the comparison value?

Why is it longer when the motor Angle reaches 360° to 0°?

0 项奖励
回复
2 回复数

4,238 次查看
KaiRiek
Contributor I
I think your configuration ist correct. You just may have a problem with showing your measurement results. I guess your measurement sampling rate ist slow and does not fit the motor speed (which is ok). So you get undersampling which leads to your described behavior.
0 项奖励
回复

4,260 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

there is a problem in reading the CNTR register value at low motor speed?

What do you mean by problem reading CNTR?

There is no restriction on reading CNTR register:

petervlna_0-1671692879332.png

Best regards,

Peter

 

0 项奖励
回复