I use MPC5745R as the main microcontroller.
A 20MHz oscillator is used and 150MHz CPU frequency is then set.
The following code runs correctly.
/************************************************************************************/
/************************************************************************************/
MC_CGM.AC3_SC.B.SELCTL=1; /*PLL0 uses an external oscillator*/
MC_CGM.AC4_SC.B.SELCTL=3; /*PLL1 source is PLL0 PHI1*/
/*20MHz XOSC->160MHz PLL0 PHI*/
/*
PLL0 PHI=Ref/(PREDIV*RFDPHI)*MFD
*/
PLLDIG.PLL0DV.B.RFDPHI = 2;
PLLDIG.PLL0DV.B.PREDIV = 1;
PLLDIG.PLL0DV.B.MFD = 16; /*8->127*/
/*
VCO_PLL0=Ref_PLL0*MFD*2/PREDIV
VCO_PLL0=20MHz*16*2/1=640MHz
*/
/*20MHz XOSC->40MHz PLL0 PHI1*/
/*
PLL0 PHI1=Ref/(PREDIV*RFDPHI1)*MFD
*/
PLLDIG.PLL0DV.B.RFDPHI1 = 8; /*4->15*/
/*40MHz PLL0 PHI1->150MHz PLL1 PHI*/
/*
PLL1 PHI=Ref*MFD/(RFDPHI*2)
*/
/*
VCO_PLL1=Ref_PLL1*MFD
VCO_PLL0=40MHz*30=1200MHz
*/
PLLDIG.PLL1DV.B.RFDPHI = 4;
PLLDIG.PLL1DV.B.MFD = 30;
/*System Clock Selector*/
MC_CGM.SC_DC[0].R = 0x80000000; /*FXBAR=150MHz*/
MC_CGM.SC_DC[1].R = 0x80010000; /*SXBAR=75MHz*/
MC_CGM.SC_DC[2].R = 0x80030000; /*PBRIDGE=37.5MHz*/
/************************************************************************************/
/************************************************************************************/
But if I change the PBRIDGE clock to 50MHz as following:
MC_CGM.SC_DC[2].R = 0x80020000; /*PBRIDGE=50MHz*/
Then my code runs wrong!!!
I don't why!
THe PBRIDGE clock must be half of the slow bar???
Thank you.
解決済! 解決策の投稿を見る。
Hi,
please look at the following table from reference manual.
This table shows, that PBRIDGE frequency has to be one quarter of system frequency (FXBAR_CLK).
Regards,
Martin
Hi,
please look at the following table from reference manual.
This table shows, that PBRIDGE frequency has to be one quarter of system frequency (FXBAR_CLK).
Regards,
Martin
Ok.
I only noticed the table 22-2 in the reference manual and ignored this table 22-3.
Thank you very much.