Hi, I have a problem with setting etpu about mpc5777c for PWMM.
I'm trying to make Double Pulse Test Code.
so, I have to control the high-side arm and low-side arm of each 3 phase respectively.
not simultaneously.
I want to modify example code for DPT test which is considering upper condition.
*base = High side, compl = Low side
this code control the high side and low side simultaneously.
only input_base_a, input_base_b, input_base_c does work.
and input_base_a, input_base_b, input_base_c these control the high side and low side simultaneously.
maybe I think there are wrong writing channel parameters.
so I'm asking for help.
Thank you.
I don't understand your question too much.
Base and complementary output runs simultaneously (with certain dead time). Pay attention to AN5374
Please clarify your question. Thanks