Hi, I'm using MPC5748G EEE module.
In SDK EEE example, there are codes that invalidate flash controller cache.
If I not using these codes, is there any problem?
From what I've tested, it seems to trigger IVOR interrupt If I don't use the above codes.
Do I always have to invalidate the flash controller cache to use EEE?
And could you give me more details about IVOR interrupt?
已解决! 转到解答。
Hi,
the buffer is invalidated automatically by interlock write. However, as mentioned in the reference manual (https://www.nxp.com/webapp/Download?colCode=MPC5748GRM
So, there should be no problem if you read EEE data only by Z4A core. If it is read also by other cores, it may lead to coherency issues.
It's not clear to me why IVOR1 is triggered. You can take a look at the core reference manual for more details:
https://www.nxp.com/webapp/Download?colCode=E200Z4RM&location=null
See Table 5-13. This can help to find more details about the source of problem. Core register MCSRR0 contains address of instruction which caused the error and MCSR contains the reason of this error.
Regards,
Lukas
Hi,
the buffer is invalidated automatically by interlock write. However, as mentioned in the reference manual (https://www.nxp.com/webapp/Download?colCode=MPC5748GRM
So, there should be no problem if you read EEE data only by Z4A core. If it is read also by other cores, it may lead to coherency issues.
It's not clear to me why IVOR1 is triggered. You can take a look at the core reference manual for more details:
https://www.nxp.com/webapp/Download?colCode=E200Z4RM&location=null
See Table 5-13. This can help to find more details about the source of problem. Core register MCSRR0 contains address of instruction which caused the error and MCSR contains the reason of this error.
Regards,
Lukas
Hi, thanks for the reply.
As you said, there are three ports on flash(MPC5748G), and each port has a read buffer.
1) Is it right that each core only can access each buffer associated with the system bus port?
- for example, Z4a I bus only can access PFLASH_0 buffer.
Z4a D bus only can access PFLASH_1 buffer.
2) In case of using EEE module only by Z2 core, is it right that I don't have to invalidate other flash controller cache(p0, p1)? (Because Z2 core only uses PFLASH_2.)