MPC5748G Debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G Debug

360件の閲覧回数
vincentbbbb
Contributor II

Hello,

 

I am trying to attach to a running application on a MPC5748G using S32DS and Multilink FX.  I am able to connect to the running device, but unable to stop the cores from running.  I hit the pause button, but I get this message: 

 

Connection from "127.0.0.1" via 127.0.0.1. Connection from port "57519" to 7224
PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @1000000 (4 bytes)

Is there something in the debug config that must be set?

 

Thanks

 

 

0 件の賞賛
返信
2 返答(返信)

347件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

342件の閲覧回数
vincentbbbb
Contributor II

I tried what is mentioned in the thread, but I get this message when I try to halt the target:

 

Interrupt command received.  Halting execution.

 

Device IDCODE is $00000082

Device ID revision is $00000000

 

Device IDCODE is $00000082

Device ID revision is $00000000

 

After that, the target restarts.

0 件の賞賛
返信