MPC5746 Internal TVS current level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5746 Internal TVS current level

ソリューションへジャンプ
1,403件の閲覧回数
RheaGao
Contributor I

Hi,

 I am using SPC5746R chip to design the minimum system with 1.25V using the following same circuit. During the debugging process, I found that 5746 would not work if I did not add Clv 1uF buffer capacitor to write the program with 200M main frequency. Specifically, I was stuck in the clock initialization and could not pass.  What mechanism triggers the microcontroller to cause this?  Thanks!

 

 

0 件の賞賛
返信
1 解決策
1,383件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Rhea,

 

Do you mean that 1uF capacitor is the only one at VDD_LV? The specification says that minumum capacitance is 4.7uF:

lukaszadrapa_0-1651474177761.png

And it’s minimal value. It should be validated by user for given application.

It is also recommended to use Progressive Clock Switching feature to avoid current spikes. Search for „Progressive Clock Switching“ in the reference manual for details.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,384件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Rhea,

 

Do you mean that 1uF capacitor is the only one at VDD_LV? The specification says that minumum capacitance is 4.7uF:

lukaszadrapa_0-1651474177761.png

And it’s minimal value. It should be validated by user for given application.

It is also recommended to use Progressive Clock Switching feature to avoid current spikes. Search for „Progressive Clock Switching“ in the reference manual for details.

Regards,

Lukas

0 件の賞賛
返信