MPC5644A BGA208 not connected pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5644A BGA208 not connected pins

814 Views
viktorfellinger
NXP Employee
NXP Employee

Dear support,

 

Automotive Customer woudl liek to use MPC5644A in MPC55xx BGA footprint.

We have a remark in our MPC5644A datasheet

 

"CAUTION
Any pins labeled “NC” are to be left unconnected. Any connection to an external circuit or
voltage may cause unpredictable device behavior or damage."

 

Now the quesion is -> is it safe to still connnect the pads below to MPC5644A 

 

Pad E13:         MPC55XX VDDE7 (3.3V)    MPC56XX NC

Pad P6: MPC55XX VDDE2 (3.3V)    MPC56XX NC

Pad P15:        MPC55XX VRC33 (3.3V)    MPC56XX NC

 

Hope you could recheck and give some guidance ...

 

Best Regards,

Viktor Fellinger

Tags (1)
0 Kudos
Reply
2 Replies

777 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Design confirmed that those pins can be connected to 3,3V or even better to the GND.

best regards,

Peter

0 Kudos
Reply

796 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello Viktor,

For future please use ticket, it is faster.

I have already consulted it with Apps engineer and we need a feedback from design as those could be test pins which should not be connected to any level or circuit.

I will contact you via email once I have any news.

Best regards,

Peter

0 Kudos
Reply