MPC5566 EMIOS SAOC mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5566 EMIOS SAOC mode

Jump to solution
308 Views
EmilyZhou8
Contributor III

Hi,

I am setting EMIOS 17 to work as SAOC mode channel which uses bus C driven by EMIOS 8. However, SAOC mode is not working. Could you please help to check my code? 

Thank you very much!

Best Regards,

Emily

#include "MPC5566.h"

/************ PWM_Period and PWM_Frequence should be changed together ************/
/* Define PWM period Counter value */
#define PWM_Period 16
#define FS_GPIO_EMIOS17 196
#define Commutation_Time_Channel FS_GPIO_EMIOS17

void initSysclk (void) {

FMPLL.SYNCR.B.LOLRE = 0; /* 0: ignore loss of lock - reset not asserted. */
FMPLL.SYNCR.B.LOLIRQ = 0; /* 0: ignore loss of lock - interrupt not requested */
FMPLL.SYNCR.B.PREDIV = 1; /* 1: use incoming OSC 8MHz / 2 = 4 MHz */
FMPLL.SYNCR.B.MFD = 28; /* 28: VCO = 4 * (28+4) = 128 MHz */
FMPLL.SYNCR.B.RFD = 1; /* 1: divide by 2, Fsys = VCO / (2^1=2) = 64MHz */
while(FMPLL.SYNSR.B.LOCK != 1){} /* Wait for FMPLL to Lock */
FMPLL.SYNCR.B.RFD = 0; /* 0: divide by 1, Fsys = VCO / (2^0=1) = 128MHz */
}

void initEMIOS(void) {
EMIOS.MCR.B.GPRE= 7; /* Divide 128 MHz sysclk by 7+1 = 8 for 16MHz eMIOS clk*/ //EMIOS.MCR.B.GPRE= 63; /* Divide 64 MHz sysclk by 63+1 = 64 for 1MHz eMIOS clk*/
EMIOS.MCR.B.ETB = 0; /* External time base is disabled; Ch 23 drives ctr bus A */
EMIOS.MCR.B.GPREN = 1; /* Enable eMIOS clock */
EMIOS.MCR.B.GTBE = 1; /* Enable global time base */
EMIOS.MCR.B.FRZ = 1; /* Enable stopping channels when in debug mode */
}

void initEMIOSch8(void) { /* EMIOS CH 8: Modulus Up Counter */
EMIOS.CH[8].CADR.R = PWM_Period - 1; /* Period will be 15+1 = 16 clocks (1 MHz) */
EMIOS.CH[8].CCR.B.MODE = 0x10; /* MPC555x: Modulus Counter (MC), internal clock */
EMIOS.CH[8].CCR.B.BSL = 0x3; /* Use internal counter */
EMIOS.CH[8].CCR.B.UCPRE=0; /* Set channel prescaler to divide by 1 */
EMIOS.CH[8].CCR.B.FREN = 1; /* Freeze channel counting when in debug mode */
EMIOS.CH[8].CCR.B.UCPREN = 1; /* Enable prescaler; uses default divide by 1 */
}

void initEMIOSch17(void) {
uint8_t EMIOS_Channel_Output;

EMIOS_Channel_Output = Commutation_Time_Channel-179; /* Convert to EMIOS channel number compatible with EMIOS struct in MPC5566.h */

EMIOS.CH[EMIOS_Channel_Output].CCR.B.MODE = 0x3; /* MPC555x: Mode is Single action output compare */
EMIOS.CH[EMIOS_Channel_Output].CCR.B.BSL = 0x1; /* Use bus C */
EMIOS.CH[EMIOS_Channel_Output].CCR.B.UCPRE = 0; /* Set channel prescaler to divide by 1 */
EMIOS.CH[EMIOS_Channel_Output].CCR.B.FREN = 1; /* Stop (freeze) channel registers when in debug mode */
EMIOS.CH[EMIOS_Channel_Output].CCR.B.UCPREN = 1; /* Enable prescaler; uses default divide by 1 */
EMIOS.CH[EMIOS_Channel_Output].CCR.B.DMA = 0; /* FLAG assigned to Interrupt request */
EMIOS.CH[EMIOS_Channel_Output].CCR.B.EDSEL = 1; /* Both edges triggering */
EMIOS.CH[EMIOS_Channel_Output].CCR.B.FCK = 0; /* Filter clock select: EMIOS clock */
EMIOS.CH[EMIOS_Channel_Output].CCR.B.IF = 0x1; /* Input filter: 8 filter clock periods */
EMIOS.CH[EMIOS_Channel_Output].CCR.B.FEN = 1; /* Flag enables interrupt */

SIU.PCR[Commutation_Time_Channel].R = 0x0E00; /* MPC555x: Initialize pad for eMIOS output */
}

void main (void) {
volatile uint32_t i = 0; /* Dummy idle counter */
uint32_t NextCmtPeriod=1000;
initSysclk(); /* Set sysclk = 128MHz running from PLL */
initEMIOS(); /* Initialize eMIOS to provide 16 MHz clock to channels */
initEMIOSch8(); /* Initialize eMIOS channel 8 as modulus counter*/
initEMIOSch17(); /* Initialize eMIOS channel 17 as SAOC, using ch 8 as time base */

while (1)
{i++;

EMIOS.CH[17].CADR.R = EMIOS.CH[8].CCNTR.R + NextCmtPeriod;
while(EMIOS.CH[17].CSR.B.FLAG != 1)
{

}
NextCmtPeriod=NextCmtPeriod+2000;
EMIOS.CH[17].CSR.B.FLAG = 1;


}
}

 

0 Kudos
Reply
1 Solution
262 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, correct.

BR, Petr

View solution in original post

0 Kudos
Reply
4 Replies
273 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you want to use local counter bus for ch17, then ch16 (counter us D) have to be configured, not ch8 you have

PetrS_0-1722834624619.png

 

BR, Petr

0 Kudos
Reply
264 Views
EmilyZhou8
Contributor III
Hi Peter,
Thanks for your reply. I am wondering if I use EMIOS Chanel 16 to set bus D, SAOC of EMIOS Channel 17 can work only if EMIOS.CH[16].CADR.R>=EMIOS.CH[17].CADR.R?

Best Regards,
Emily
0 Kudos
Reply
263 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, correct.

BR, Petr

0 Kudos
Reply
226 Views
EmilyZhou8
Contributor III
Thanks a lot!
0 Kudos
Reply