I am looking for driver software to program and erase the flash in a PXN20. I noticed the twrpxn20 bsp in mqx points to flash_c90.c. Is C90 a family of flash? Is the following compatible with the PXN20?
MPC5674F_C90FL_SSD_DRV: MPC5674F-5676R C90FL Flash Standard
Software Driver.
Size (K): 5294
Format: exe Rev #: 1.0.2 Modified: 8/6/2013
If not does a generic flash driver exist?
Thanks,
Ed
Hi,
they are not compatible.
Please go to the page:
Go down and find Run-time Software; Expand it and you can see two drivers for this MCU.:
C90FL_SM_SSD_DEVD: MPC56xx C90FL Standard Software Driver for
Single-Module Flash.
Size (K): 4891
Format: exe Rev #: 1.0.2 Modified: 8/6/2013
MPC56xx C90FL EEPROM Emulation Software Driver: MPC56xx C90FL EEPROM Emulation Software Driver
Size (K):
5689 Format: exe Rev #: 1.0.5 Modified: 5/16/2013
Best regards,
Ladislav