Is the MPC5674F-5676R C90FL Flash Standard Software Driver compatible with the PXN20?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is the MPC5674F-5676R C90FL Flash Standard Software Driver compatible with the PXN20?

1,684 次查看
edwarddarosa
Contributor II

I am looking for driver software to program and erase the flash in a PXN20. I noticed the twrpxn20 bsp in mqx points to flash_c90.c. Is C90 a family of flash? Is the following compatible with the PXN20?

 

MPC5674F_C90FL_SSD_DRV: MPC5674F-5676R C90FL Flash Standard

Software Driver.

Size (K): 5294
Format: exe Rev #: 1.0.2 Modified: 8/6/2013

 

If not does a generic flash driver exist?

 

Thanks,

Ed

标签 (1)
标记 (2)
1 回复

1,009 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

they are not compatible.

Please go to the page:

MPC5668G Product Summary Page

Go down and find Run-time Software; Expand it and you can see two drivers for this MCU.:

C90FL_SM_SSD_DEVD: MPC56xx C90FL Standard Software Driver for

Single-Module Flash.

Size (K): 4891
Format: exe Rev #: 1.0.2 Modified: 8/6/2013

MPC56xx C90FL EEPROM Emulation Software Driver: MPC56xx C90FL EEPROM Emulation Software Driver

Size (K):
5689 Format: exe Rev #: 1.0.5 Modified: 5/16/2013

Best regards,

Ladislav

0 项奖励
回复