Get the actual flash size of the device MPC57xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Get the actual flash size of the device MPC57xx

Jump to solution
1,361 Views
riccardo_ertolu
Contributor II

Hello everybody,

I am looking for a way to get the actual size of the flash memory available inside the device.

I was looking at MIDR2, but it is not clear if that value is just the maximum size available for the biggest device of that family.

Let's consider MPC5746C and MPC5745B, do they have different values on MIDR2?

riccardo_ertolu_0-1627751045539.png

Thanks in advance

Tags (1)
0 Kudos
Reply
1 Solution
1,319 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

MPC574xR supports it, in the MIDR fields partnumber as well as flash size fits to its sub-derivatives i.e. to ordering part number.

MPC574xP has it implemented as well but a bit different way, it is encoded in MIDR2 register, whilst MIDR1 still says 5744. Memory size correlates with 5744/3/2/1 value as shown in the screenshot below:

davidtosenovjan_0-1628249590145.png

 

View solution in original post

4 Replies
1,340 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, unfortunately this device does not allow to distinguish between sub-derivatives SW way.

MIDR specifies only two families MPC5746C and MPC5748G and their subset devices have the same MIDR content.

1,324 Views
riccardo_ertolu
Contributor II

Thanks for the info.

What about other similar devices, such as Panther MPC574xP or Rainer MPC574xR?

Thanks

0 Kudos
Reply
1,320 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

MPC574xR supports it, in the MIDR fields partnumber as well as flash size fits to its sub-derivatives i.e. to ordering part number.

MPC574xP has it implemented as well but a bit different way, it is encoded in MIDR2 register, whilst MIDR1 still says 5744. Memory size correlates with 5744/3/2/1 value as shown in the screenshot below:

davidtosenovjan_0-1628249590145.png

 

1,313 Views
riccardo_ertolu
Contributor II

Thanks!

0 Kudos
Reply