Cannot find "e_li" in e200z4RM.pdf

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot find "e_li" in e200z4RM.pdf

Jump to solution
3,442 Views
zhanglei327
Contributor II

I cannot find e_li in e200z4RM.pdf. Where can I find it? Im using SPC5646B. Thank you!

e_li.png

Tags (1)
1 Solution
3,071 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

please check the document in the post attachment.

Regards,

Martin

View solution in original post

0 Kudos
Reply
7 Replies
3,072 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

please check the document in the post attachment.

Regards,

Martin

0 Kudos
Reply
3,071 Views
zhanglei327
Contributor II

I cannot find the "mtlr" in "VLEPEM.pdf", but I find the "se_mtlr" in "VLEPEM.pdf". Are they same? Thank you!

se_mtlr.jpg

mtlr.jpg

0 Kudos
Reply
3,071 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

instructions which starts with e_ or se_ are from VLE instruction set. Instructions without e_ or se_ are BookE instructions.

For more information about BookE instructions, please check the document in the attachment.

Regards,

Martin

3,071 Views
zhanglei327
Contributor II

I searched the "mtlr" in the "EREFRM_2-0.pdf", but I still cannot find it. Thank you!

0 Kudos
Reply
3,071 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

sorry my mistake. In BookE, there is only mtspr instruction, so it seems mtlr is alias to mtspr instruction, because Link register is also marked as spr x register.

Instruction mtld loads data to link register as well as se_mtlr.

Regards,

Martin

3,071 Views
zhanglei327
Contributor II

mtlr only has one parameter, but mtspr has two parameter. Thank you!

se_mtlr.jpg

mtspr.JPG

0 Kudos
Reply
3,071 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

As I wrote you before. mtlr is only mnemonic to mtspr instruction. Please check for example the link below:

PowerPC Instruction Set: mtspr 

pastedImage_3.png

Regards,

Martin