Autosar-compliant Multicore on MPC5777M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Autosar-compliant Multicore on MPC5777M

ソリューションへジャンプ
2,109件の閲覧回数
littledino2112
Contributor I

Hi guys,

Based on Autosar multicore concept, there need to be one 'master' core booting up first, then the master core will command the slave core(s) to start. From what i understand from the MPC5777M RM, the cores are started by setting the RCHW, which means all the cores are booted up at the same time once the BAF code reads this RCHW during start-up. So my question is How can i apply the concept of Autosar here with the MPC5777M? How can I start one core after startup then decide when to start the other cores if needed?

 

Regards,

Hoang

ラベル(1)
タグ(2)
1 解決策
1,705件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

MPC5777M after reset starts only with peripheral core active (IO core) - core2.

The idea is to give user a space to initialize all safety critical mechanisms (self-tests, measurements, etc..) before main cores with safety tasks are released from reset. User has to start(release from reset) additional cores manually by SW like in my example which Tomas linked.

Your AUTOSAR OS will be running from one of the main cores, core0 or core1. Safety critical application will run from core0 which is lockstepped by core0s.

But it is fully on user how he will use the cores.

Peter

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,705件の閲覧回数
thomasolenik
Contributor III

My understanding is that core2 needs to set the clocks then boots core0 and core1. Take a look at this example:

Example MPC5777M-DPM-PLL-200MHz

1,706件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

MPC5777M after reset starts only with peripheral core active (IO core) - core2.

The idea is to give user a space to initialize all safety critical mechanisms (self-tests, measurements, etc..) before main cores with safety tasks are released from reset. User has to start(release from reset) additional cores manually by SW like in my example which Tomas linked.

Your AUTOSAR OS will be running from one of the main cores, core0 or core1. Safety critical application will run from core0 which is lockstepped by core0s.

But it is fully on user how he will use the cores.

Peter

0 件の賞賛
返信
1,705件の閲覧回数
littledino2112
Contributor I

Thanks Peter and Thomas,

The attached example does answer my question about the multicore bootup process.

Hoang

0 件の賞賛
返信