********************************************************************************
* Detailed Description:
* In case user want GHS to initialize all cores it is necessary to define
* preprocessor symbol: init_cores
* However in this example the cores are initialized from function: Core_Boot();
* This example demonstrates how to initialize clock module and activate core0, core1 and core0 locksteped core.
* ------------------------------------------------------------------------------
* Test HW: MPC57xx EVB
* Maskset: 0N78H
* Target : internal_FLASH
* Fsys: 200 MHz PLL
*
********************************************************************************
Revision History:
1.0 Feb-08-2016 b21190(Vlna Peter) Initial Version
1.1 Feb-09-2016 b21190(Vlna Peter) Added Core_Boot() function
*******************************************************************************/