An error occurs when the bus load rate is relatively high before the mpc5748g is powered on and the can interface is initialized

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

An error occurs when the bus load rate is relatively high before the mpc5748g is powered on and the can interface is initialized

613 Views
dazhou0503
Contributor I
微信图片_20200122174900.pngvoid flexcan_callback(uint8_t instance, flexcan_event_type_t eventType,
       uint32_t buffIdx, flexcan_state_t *flexcanState)
{
 //BaseType_t status;
 struct RECV_CAN_DATA frame;
#if 0
 if (FLEXCAN_EVENT_RX_COMPLETE == eventType)
 {
  switch(instance)
  {
   case INST_CANCOM1 :
    FLEXCAN_DRV_Receive(INST_CANCOM1, 1, &recv_buff[0]);
    frame.channel =1;
   break;
   case INST_CANCOM2:
    FLEXCAN_DRV_Receive(INST_CANCOM2, 1, &recv_buff[0]);
    frame.channel =2;
    break;
   case INST_CANCOM3 :
    FLEXCAN_DRV_Receive(INST_CANCOM3, 1, &recv_buff[0]);
    frame.channel =3;
   break;
   case INST_CANCOM4 :
    FLEXCAN_DRV_Receive(INST_CANCOM4, 1, &recv_buff[0]);
    frame.channel =4;
    break;
   case INST_CANCOM5 :
    FLEXCAN_DRV_Receive(INST_CANCOM5, 1, &recv_buff[0]);
    frame.channel =5;
    break;
   default:
   break;
  }
#ifdef FREERTOS
  frame.relative_time = PIT_DRV_GetCurrentTimerUs(INST_PIT1,0);
  frame.canId = recv_buff[0].msgId;
  memcpy(frame.can_data,recv_buff[0].data,8);
  status = xQueueSendToBackFromISR(rcv_queue,(void *const)&frame,pdTRUE);
  if(status != pdPASS)
  {
  }
#else if
  frame_data[write_pstr].relative_time = PIT_DRV_GetCurrentTimerUs(INST_PIT1,0);
  frame_data[write_pstr].canId = recv_buff[0].msgId;
  memcpy(frame_data[write_pstr].can_data,recv_buff[0].data,8);
  write_pstr++;
  if(write_pstr>=100)
   write_pstr=0;
#endif
 }
#endif
 if (FLEXCAN_EVENT_RXFIFO_COMPLETE == eventType)
 {
  switch(instance)
  {
   case INST_CANCOM1 :
    FLEXCAN_DRV_RxFifo(INST_CANCOM1,&recv_buff[0]);
    frame_data[write_pstr].channel =1;
   break;
   case INST_CANCOM2:
    FLEXCAN_DRV_RxFifo(INST_CANCOM2,&recv_buff[0]);
    frame_data[write_pstr].channel =2;
    break;
   case INST_CANCOM3 :
    FLEXCAN_DRV_RxFifo(INST_CANCOM3,&recv_buff[0]);
    frame_data[write_pstr].channel =3;
   break;
   case INST_CANCOM4 :
    FLEXCAN_DRV_RxFifo(INST_CANCOM4,&recv_buff[0]);
    frame_data[write_pstr].channel =4;
    break;
   case INST_CANCOM5 :
    FLEXCAN_DRV_RxFifo(INST_CANCOM5,&recv_buff[0]);
    frame_data[write_pstr].channel =5;
    break;
   default:
   break;
  }
  time_count = xTaskGetTickCountFromISR() - create_file_time_count;
  if(write_pstr == read_pstr)
   write_pstr = read_pstr=0;
  frame_data[write_pstr].relative_time = time_count;
  frame_data[write_pstr].canId = recv_buff[0].msgId;
  memcpy(frame_data[write_pstr].can_data,recv_buff[0].data,8);
  write_pstr++;
  /*
  if(recv_buff[0].msgId == PP7_TIME_CANID)
  {
   memcpy(&real_time,recv_buff[0].data,8);
  }
  */
  if(write_pstr>=MAX_CAN_FRAME_LEN)
   write_pstr=0;
 }
}
/*
 * @brief: Send data via CAN to the specified mailbox with the specified message id
 * @param mailbox   : Destination mailbox number
 * @param messageId : Message ID
 * @param data      : Pointer to the TX data
 * @param len       : Length of the TX data
 * @return          : None
 */
void send_can_data(uint32_t mailbox, uint32_t messageId, uint8_t *data, uint32_t len)
{
    /* Set information about the data to be sent
     *  - 1 byte in length
     *  - Standard message ID
     *  - Bit rate switch enabled to use a different bitrate for the data segment
     *  - Flexible data rate enabled
     *  - Use zeros for FD padding
     */
    flexcan_data_info_t dataInfo =
    {
  .data_length = len,
  .msg_id_type = FLEXCAN_MSG_ID_STD,
  .enable_brs = false,
  .fd_enable = false,
  .fd_padding = 0U};
    /* Configure TX message buffer with index TX_MSG_ID and TX_MAILBOX*/
    FLEXCAN_DRV_ConfigTxMb(INST_CANCOM1, mailbox, &dataInfo, messageId);
    /* Execute send non-blocking */
    FLEXCAN_DRV_Send(INST_CANCOM1, mailbox, &dataInfo, messageId, data);
}
void can_set_filter(uint8_t instance,flexcan_msgbuff_id_type_t idType,uint32_t buffIdx,uint32_t mask)
{
 uint16_t id_counter;
    /* Check buffer index to avoid overflow */
    DEV_ASSERT(buffIdx < FEATURE_CAN_MAX_MB_NUM);
 for(id_counter=0;id_counter<16;id_counter++)
 {
  filterTable[id_counter].isRemoteFrame = false;
  filterTable[id_counter].isExtendedFrame = false;
  filterTable[id_counter].id = id_counter +1 ;
 }
 /* Configure RX FIFO ID filter table elements based on filter table defined above*/
 FLEXCAN_DRV_ConfigRxFifo(instance, FLEXCAN_RX_FIFO_ID_FORMAT_A, filterTable);
 FLEXCAN_DRV_SetRxMaskType(instance,FLEXCAN_RX_MASK_INDIVIDUAL);
 for(id_counter=0;id_counter<10;id_counter++)
  FLEXCAN_DRV_SetRxIndividualMask(instance, FLEXCAN_MSG_ID_EXT, id_counter, 0);
 /* rest of filter items are masked with RXFGMASK */
 FLEXCAN_DRV_SetRxFifoGlobalMask(instance, FLEXCAN_MSG_ID_STD, 0);
}
void can_cfg_rx_mb(uint8_t instance, uint8_t mb_idx, uint32_t msgid)
{
 flexcan_data_info_t rx_info =
 {
  .data_length = 8U,
  .msg_id_type = FLEXCAN_MSG_ID_STD,
  .enable_brs = false,
  .fd_enable = false,
  .fd_padding = 0U
 };
 FLEXCAN_DRV_ConfigRxMb(instance, mb_idx, &rx_info, msgid);
}
void can_dev_init()
{
 INT_SYS_DisableIRQGlobal();
 FLEXCAN_DRV_Init(INST_CANCOM1, &canCom1_State, &canCom1_InitConfig0);
 FLEXCAN_DRV_Init(INST_CANCOM2, &canCom2_State, &canCom2_InitConfig0);
 FLEXCAN_DRV_Init(INST_CANCOM3, &canCom3_State, &canCom3_InitConfig0);
 FLEXCAN_DRV_Init(INST_CANCOM4, &canCom4_State, &canCom4_InitConfig0);
 FLEXCAN_DRV_Init(INST_CANCOM5, &canCom5_State, &canCom5_InitConfig0);
 can_cfg_rx_mb(INST_CANCOM1, 1, 0);
 can_cfg_rx_mb(INST_CANCOM2, 1, 0);
 can_cfg_rx_mb(INST_CANCOM3, 1, 0);
 can_cfg_rx_mb(INST_CANCOM4, 1, 0);
 can_cfg_rx_mb(INST_CANCOM5, 1, 0);
 can_set_filter(INST_CANCOM1,FLEXCAN_MSG_ID_EXT,0,0);
 can_set_filter(INST_CANCOM2,FLEXCAN_MSG_ID_EXT,0,0);
 can_set_filter(INST_CANCOM4,FLEXCAN_MSG_ID_EXT,0,0);
 can_set_filter(INST_CANCOM5,FLEXCAN_MSG_ID_EXT,0,0);
 can_set_filter(INST_CANCOM3,FLEXCAN_MSG_ID_EXT,0,0);
 FLEXCAN_DRV_InstallEventCallback(INST_CANCOM1, flexcan_callback, ((void *)0));
 FLEXCAN_DRV_InstallEventCallback(INST_CANCOM2, flexcan_callback, ((void *)0));
 FLEXCAN_DRV_InstallEventCallback(INST_CANCOM3, flexcan_callback, ((void *)0));
 FLEXCAN_DRV_InstallEventCallback(INST_CANCOM4, flexcan_callback, ((void *)0));
 FLEXCAN_DRV_InstallEventCallback(INST_CANCOM5, flexcan_callback, ((void *)0));
 /*
 FLEXCAN_DRV_Receive(INST_CANCOM1, 1, &recv_buff[0]);
 FLEXCAN_DRV_Receive(INST_CANCOM2, 1, &recv_buff[1]);
 FLEXCAN_DRV_Receive(INST_CANCOM3, 1, &recv_buff[2]);
 FLEXCAN_DRV_Receive(INST_CANCOM4, 1, &recv_buff[3]);
 FLEXCAN_DRV_Receive(INST_CANCOM5, 1, &recv_buff[4]);
*/
 FLEXCAN_DRV_RxFifo(INST_CANCOM1,&recv_buff[0]);
 FLEXCAN_DRV_RxFifo(INST_CANCOM2,&recv_buff[1]);
 FLEXCAN_DRV_RxFifo(INST_CANCOM3,&recv_buff[2]);
 FLEXCAN_DRV_RxFifo(INST_CANCOM4,&recv_buff[3]);
 FLEXCAN_DRV_RxFifo(INST_CANCOM5,&recv_buff[4]);
 INT_SYS_EnableIRQGlobal();
}
0 Kudos
Reply
1 Reply

553 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the error shown on Expression window could be caused due to Local variables displayed.

Next, the code seems to be stopped on Wake-up interrupt, this could be caused if Wake-up interrupt is enabled for a pin that is connected to CAN transceiver and there is communication on the bus. You should be able to inspect which WKUP source is asserted.

BR, Petr  

0 Kudos
Reply