Hi,
I want to connect 5v to an ADC channel and read the ADC count. Which example in MPC5777C is suitable for this. Please suggest.
Thanks and Regards
Krishna
I can recommend for instance following:
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5-software-example-list/ta-p/1102445#MPC5777C
Example MPC5777C eMIOS-eQADC Continuous external trigger mode GHS614
Example MPC5777C-SDADC_simple GHS614
Example MPC5777C-SDADC_eTPU_triggered GHS714
Example MPC5777C-eQADC_Simple GHS714
Example MPC5777C-eQADC_Simple+Calibration GHS714
Example MPC5777C eQADC_Simple+Calibration+Timestamp GHS714
Example MPC5777C-eQADC_A+B-Calibration GHS714
or any example related to MPC5777C (also S32 Design Studio may offer software examples)