ASIL D for MPC5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ASIL D for MPC5777C

Jump to solution
1,182 Views
berat24
Contributor III

Hello everyone,

MPC5777C supports realibity up to ASIL D powertrain. How can we prove that We use ASIL-D supported features of the MCU?

MPC5xxx Microcontrollers | NXP Semiconductors

0 Kudos
Reply
1 Solution
1,166 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Functional safety and the ISO26262 standard define the general guidelines needed to fulfill the requirements for the different ASIL levels. In NXP we have a program called safe assure. For more information about this program and the devices see following link:

https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTN...

“The SafeAssure program highlights selected solutions - including hardware and software - that are targeted for use in functional safety applications, enabling system designers to design with confidence and achieve their system-level design goals and standards compliance more efficiently.”

ASIL certification is being above whole ECU/system level, so customer could develop ASIL-D compliant appliance with MPC5777C (he could also develop ASIL-D compliant appliance with other devices than safety certified, but such approach could be in-efficient, slow, expensive, complicated, and so on…)

It means not only MCU is designed and manufactured according ISO26262 requirements (safety HW) but also we are providing safety software and safety support (documents) as stated on the link above.

Here you may find procedure how to obtain safety documents:

https://community.nxp.com/t5/SafeAssure-Community/bd-p/safeassure

View solution in original post

0 Kudos
Reply
1 Reply
1,167 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Functional safety and the ISO26262 standard define the general guidelines needed to fulfill the requirements for the different ASIL levels. In NXP we have a program called safe assure. For more information about this program and the devices see following link:

https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTN...

“The SafeAssure program highlights selected solutions - including hardware and software - that are targeted for use in functional safety applications, enabling system designers to design with confidence and achieve their system-level design goals and standards compliance more efficiently.”

ASIL certification is being above whole ECU/system level, so customer could develop ASIL-D compliant appliance with MPC5777C (he could also develop ASIL-D compliant appliance with other devices than safety certified, but such approach could be in-efficient, slow, expensive, complicated, and so on…)

It means not only MCU is designed and manufactured according ISO26262 requirements (safety HW) but also we are providing safety software and safety support (documents) as stated on the link above.

Here you may find procedure how to obtain safety documents:

https://community.nxp.com/t5/SafeAssure-Community/bd-p/safeassure

0 Kudos
Reply