MPC5xxx ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5xxx Knowledge Base

ラベル
  • General 164
  • test 7

ディスカッション

ソート順:
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed frequency (48MHz) * Setup SIU, and demonstrate frequency modulation. * ------------------------------------------------------------------------------ * Test HW:        XPC560B 64LQFP, XPC56XX EVB MOTHEBOARD Rev.C * MCU:             SPC5602D * Cut:               1M18Y * Fsys:             48 MHz * Debugger:     Lauterbach Trace32 * Target:           internal_FLASH * EVB clkout pin : Port J7 - pin 0 * ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * * Configures the FlexCAN to transmit and receive a CAN message. * ECC reporting in the FlexCAN module is disabled. * * In this config, CAN_A transmits a message. CAN_B receives the message. * CAN_A MB8 is configured to send data. CAN_A sends message each 1sec. * This interval is generated by PIT. * CAN_B MB9 is configured to receive a message, SW polling is used. * * Connect CAN0-CANH on P15-1 to CAN1-CANH on P14-1 * Connect CAN0-CANL on P15-2 to CAN1-CANL on P14-2 * * * ------------------------------------------------------------------------------ * Test HW:         MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU:             PPC5777CMM03 2N45H CTZZS1521A * Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A *           use USB connector (J21) on minimodule * * EVB connection:  ETPUA30 (PortP P23-15) --> USER_LED_1 (P7-1) *                  ETPUA31 (PortP P23-14) --> USER_LED_2 (P7-2) * ********************************************************************************
記事全体を表示
WARNING 1: Use censorship feature very carefully, because an inappropriate usage can lead in making the device useless!!! Thoroughly read all instructions before use!!!   WARNING 2: Version of ICDPPCNEXUS debugger that is included with CodeWarrior 2.10 is not capable to enable debug on certain devices including MPC5604B. Workaround is either using of Codewarrior 10.6 or using of PKGPPCNEXUS debugger - can be downloaded from P&E Microcomputer Systems   WARNING 3: In case TRACE32 debugger is being used (Lauterbach), it is needed to have updated TRACE32 software. TRACE32 releases 02/2015 and 09/2016..02/2018 may not be able to access to censored device. LAUTERBACH DEVELOPMENT TOOLS   The example consists of 2 parts and document describing how to access censored device via JTAG with using of PeMicro or Lauterbach debugger:   1) MPC5604B-Censor_device-CW210: ******************************************************************************** * Detailed Description: * The example code reprogram content of shadow flash to enable censorship. * After succesful operation LED1 is lighting. After power-on-reset the device * is censored with private 0xFEED_FACE_CAFE_BEEF. Subsequently the access can be * allowed by enabling debug of censored device as decipted in attached pdf * document. On this device password must be entered in reverse order i.e. * 0xCAFE_BEEF_FEED_FACE. Shadow flash re-programming code must be executed from * internal RAM. * ------------------------------------------------------------------------------   2) MPC5604B-Uncensor_device-CW210: ******************************************************************************** * Detailed Description: * Supposing the device is censored by example MPC5604B-Censor_device-CW210 * Firstly it is needed to enabled debug of censored device as decipted in * attached pdf document. On this device password must be entered in reverse * order i.e.0xCAFE_BEEF_FEED_FACE. MPC5604B_run_from_ram.cmm script does it by * command SYStem.option.keycode 0xCAFEBEEFFEEDFACE. * Then run this code to uncensor the device. After succesful operation LED1 is * lighting. After power-on-reset the device is uncensored and subsequent access * will be without password. Shadow flash re-programming code must be executed * from internal RAM. * ------------------------------------------------------------------------------
記事全体を表示
******************************************************************************** * Detailed Description: * * Configure the device to wake up by STM_0 timer. * Configure the device to enter STANDBY mode from DRUN * Once the device is woken up by STM_0, the device is restared becase * we wrote address of entry point to register MC_ME.CADDR[1].R * ------------------------------------------------------------------------------ * Test HW:         MPC574XG-324DS Rev.A + MPC574XG-MB Rev.C * MCU:             PPC5748GMMN6A 1N81M * Fsys:            Default * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * * This example shows how to use CRC module. * - CRC32 is used * - byte stream is written into input register * - one test case uses direct access to CRC registers * - second test case uses DMA to write the data stream * - the results can be compared using this online calculator: *   http://www.zorc.breitbandkatze.de/crc.html * - screenshots from online calculator are attached * ------------------------------------------------------------------------------ * Test HW:         MPC574XG-324DS Rev.A + MPC574XG-MB Rev.C * MCU:             PPC5748GMMN6A 1N81M * Fsys:            160 MHz PLL * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * This example shows, how to use interrupt hardware vector mode. In the example * PIT0 interrupt and external interrupt source 1 are implemented. PIT interrupt * toggle LED every second, external interrupt causes IVOR1 exception. * * This example also shows, how to use exceptions, while HW vector mode is used. * After SW1 button is pressed, uninitialized RAM is read and IVOR1 exception is * reached. In IVOR1, only endless loop is implemented and micro has to be reset * externally if you want to get out from this loop. * * * For correct HW vector mode setup, following files was added to the project: * *  - exceptions.s *  - handlers_vle.s *  - HW_vector.c * * * Following files was modified (all changes are marked by comment): * *  - mem.ld *  - sections.ld *  - Vector.c *  - MPC57xx__Interrupt_Init.c * * *  Following files was removed from project (files are still place in project, but *  not compiled and linked) * *  - intc_sw_handlers.S *  - intc_SW_mode_isr_vectors_MPC5744P.c * * * * Test HW:         X-MPC5744P-144DC, MPC57xx motherboard * MCU:             PPC5744PFMLQ8 0N15P * Fsys:            200 MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH (debug mode, release mode) * EVB connection:  User LED 1 connected to A0 (P8.0), *                    User switch SW1 connected to A1 (P8.1) * * * ------------------------------------------------------------------------------ * ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * Example demonstates Shifted PWM generating via eMIOS. * The shift is 25% duty cycle. * ------------------------------------------------------------------------------ * Test HW:  MPC5644A + XPC564A minimodule + XPC56XX mother board * Maskset:  OM14X * Target :  Internal Flash * Fsys:     16MHz IRC * * EVB settings: * PJ8 pin 0 is eMIOS CH[0] * PJ8 pin 2 is eMIOS CH[2] ******************************************************************************** Revision History: 1.0     Jun-23-2016     b21190(Vlna Peter)  Initial Version *******************************************************************************/
記事全体を表示
******************************************************************************** * Detailed Description: * Example configures LinFlex and eDMA modules and then periodically sends notice * to the terminal window (19200-8-no parity-1 stop bit-no flow control). * * ------------------------------------------------------------------------------ * Test HW:         MPC5607BEVB * Target :         internal_FLASH, RAM * Terminal:        19200-8-no parity-1 stop bit-no flow control * Fsys:            40 MHz PLL with 8 MHz crystal reference * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Terminal:        19200-8-no parity-1 stop bit-no flow control via LINFlex0 * EVB connection:  default * ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, blinking one LED by interrupt, second LED by software * loop, third LED by second core, initializes and display notice via UART * terminal and then terminal ECHO. * * ------------------------------------------------------------------------------ * Test HW:  XPC56xxMB2 + XPC564xB/C, PPC5646C 0M87Y silicon * Target :  internal_FLASH, RAM * Fsys:     120 MHz PLL0 * Debugger: Lauterbach Trace32. script for internal_FALSH run_from_flash.cmm *                               script for RAM: run_from_ram_vle.cmm * ********************************************************************************
記事全体を表示
Demo application MPC5606S-DEMO + LM75B + HIH-5030 + PCA8565 + GUI Simple weather station demo using 2 external sensors and  external real time clock/calendar   For detailed description SEE ATTACHED document. ------------------------------------------------------------------------------ Test HW:            MPC5606S-DEMO-V2 + LM75BD + HIH-5030 + PCA8565 sensors MCU:             PPC5606SEF OMLU 0M25V DD68391 XOTAC1003 Fsys:            64MHz Debugger:        Lauterbach Trace32 Target:          internal_FLASH Terminal:        none EVB connection:  1) Temperature sensor LM75B:                        J51.40 - F[6] -> LM75B SDA                        J51.43 - F[7] -> LM75B SCL                        J52.1  - 3.3V -> LM75B Vcc                        J50.1  - GND  -> LM75B Gnd                   2) Humidity sensor HIH-5030:                        J52.1  - 3.3V -> HIH-5030 Ve+                        J50.1  - GND  -> HIH-5030 Ve-                        J50.1  - ANS0 -> HIH-5030 Out                   3) External Real Time Clock:                        J51.40 - F[6] -> PCA8565 SDA                        J51.43 - F[7] -> PCA8565 SCL                        J52.1  - 3.3V -> PCA8565 Vcc                        J50.1  - GND  -> PCA8565 Gnd                                        *******************************************************************************
記事全体を表示
Detailed Description: Demo application performs I2C communication with externally connected external real time clock/calendar PCA8565. Obtained values and processed and displayed on MPC5606S-DEMO-V2 board’s TFT panel. Date and time may be set up by demo board’s buttons (SW2-SW6). Application uses standard Graphics Libraries for MPC5606S for simple graphic output that is managed in mc_base.c module only. I2C communication is managed with using of own two layer driver where low-level driver consisting of I2C_0.c and I2C_0.h - these can be used for any device connected to I2C_0 module. Middle-level driver layer consist of I2C_PCA8565.c and I2C_PCA8565.h and it is specific to PCA8565 device. ------------------------------------------------------------------------------ Test HW:            MPC5606S-DEMO-V2 + LM75BD + HIH-5030 + PCA8565 sensors MCU:             PPC5606SEF OMLU 0M25V DD68391 XOTAC1003 Fsys:            64MHz Debugger:        Lauterbach Trace32 Target:          internal_FLASH Terminal:        none EVB connection:   For complete project you may see following link: Demo application MPC5606S-DEMO + LM75B + HIH-5030 + PCA8565 + GUI
記事全体を表示
Detailed Description: Demo application performs I2C communication with externally connected temperature sensor LM75B. Obtained values and processed and displayed on MPC5606S-DEMO-V2 board’s TFT panel. Application uses standard Graphics Libraries for MPC5606S for simple graphic output that is managed in mc_base.c module only. I2C communication is managed with using of own two layer driver where low-level driver consisting of I2C_0.c and I2C_0.h - these can be used for any device connected to I2C_0 module. Middle-level driver layer consist of I2C_LM75B.c and I2C_LM75B.h and it is specific to LM75B device. ------------------------------------------------------------------------------ Test HW:            MPC5606S-DEMO-V2 + LM75BD MCU:             PPC5606SEF OMLU 0M25V DD68391 XOTAC1003 Fsys:            64MHz Debugger:        Lauterbach Trace32 Target:          internal_FLASH Terminal:        none EVB connection:   For complete project you may see following link: Demo application MPC5606S-DEMO + LM75B + HIH-5030 + PCA8565 + GUI
記事全体を表示
Detailed Description: Demo application measures analog voltage from externally connected humidity sensor HIH-5030. Obtained values and processed and displayed on MPC5606S-DEMO-V2 board’s TFT panel. Application uses standard Graphics Libraries for MPC5606S for simple graphic output that is managed in mc_base.c module only. ------------------------------------------------------------------------------ Test HW:            MPC5606S-DEMO-V2 + HIH-5030 MCU:             PPC5606SEF OMLU 0M25V DD68391 XOTAC1003 Fsys:            64MHz Debugger:        Lauterbach Trace32 Target:          internal_FLASH Terminal:        none EVB connection:   For complete project you may see following link: Demo application MPC5606S-DEMO + LM75B + HIH-5030 + PCA8565 + GUI
記事全体を表示
******************************************************************************** * Detailed Description: * This example demonstrates how to configure (CGM) clock generation module * and supply by clock all main peripherals. * ------------------------------------------------------------------------------ * Test HW:  MPC57xx Motherboard + MPC5746R_176DC minimodule, MPC5746R * Maskset:  1N83M (cut 2.0B) * Target :  internal_FLASH * Fsys:     200MHz PLL0 as system clock ******************************************************************************** Revision History: 1.0     Oct-19-2015     b21190(Vlna Peter)  Initial Version 1.1    Nov-11-2015    b21190(Vlna Peter)  Added PPL0 200MHz as system clock 1.2    Dec-02-2015    b21190(Vlna Peter)  Added Flash controller init 1.3    Dec-02-2015    b21190(Vlna Peter)  Fixed system clock init 1.4    Feb-07-2017    b21190(Vlna Peter)  SWT0 and SWT1 disabled in startup *******************************************************************************/
記事全体を表示
******************************************************************************** * Detailed Description: * Sensor board OM11057A which includes two PCF8885 circuits is connected * to MPC5748G via I2C. MPC5748G continuously reads the state of touch sensors * and the state is shown on LED diodes which are driven by I2C circuit PCA9535. * * Used I2C driver: https://community.freescale.com/docs/DOC-330972 * * Touch sensor board (page 9 and 10): * http://www.nxp.com/documents/user_manual/UM10505.pdf * * ------------------------------------------------------------------------------ * * Connection: * * Connect I2C bus (I2C_2 on MPC5748G) to sensor board: * I2C_SCL: P24-33 (pin PE9) on MPC574XG-MB to K3-1 on OM11057A * I2C_SDA: P24-35 (pin PE8) on MPC574XG-MB to K3-13 on OM11057A * Note: use two pull-up resistors on I2C signals (pulled to 3.3V). * The value should be 3k3 - 10k * * Connect power supply from MPC574XG-MB to OM11057A: * GND: P24-2 on MPC574XG-MB to K3-7 on OM11057A * 3.3V: P24-1 on MPC574XG-MB to K3-9 on OM11057A * * Connect SLEEP pins of both PCF8885 to GND (this will ensure that sleep mode * is not entered): * SLEEP1: K3-11 to K2-3 (both on OM11057A) * SLEEP2: K1-6 to K1-8 (both on OM11057A) * * ------------------------------------------------------------------------------ * Sensor board:    OM11057A *                  http://www.nxp.com/documents/user_manual/UM10505.pdf * Test HW:         MPC574XG-324DS Rev.A + MPC574XG-MB Rev.C * MCU:             PPC5748GMMN6A 1N81M * Fsys:            160 MHz PLL * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * ********************************************************************************
記事全体を表示
This document summarizes simple I2C driver implementation for MPC5xxx devices. The code follows Reference Manual's Flow-Chart of Typical I2C Interrupt Routine.
記事全体を表示
******************************************************************************** * Detailed Description: * Used flash driver:  MPC5700 C55FG Flash Standard Software Driver (REV 1.1.0) * http://www.nxp.com/files/product/software/C55_JDP_SSD.exe * * This example checks four large 256KB flash blocks at address 0x0100_0000 - * 0x010F_FFFF. * Some random data are placed to this section (constant "flash_data[]"), so the * s-record is not empty. * It is necessary to use off-line MISR_C55.exe tool which calculates MISR * values for selected flash blocks. See the "MISR gen" folder included in this * project. File "core0.run" is s-record file which is used for calculation. It * contains the data (constant "flash_data[]") placed to the selected blocks. * "misr.bat" file shows how to call the calculator. * "output.txt" contains the result of this operation - the MISR values. * Once this is done, initialize the SSD drivers, unlock blocks which are going * to be checked and run the FlashArrayIntegrityCheck function. * Notice that the code must be executed from RAM. We cannot access the flash * during this operation. If the operation is successful, FlashCheckStatus will * return opResult C55_OK if the MISR values are equal. It will return * C55_ERROR_MISMATCH if the MISR values are not equal, i.e. the flash is * corrupted and the content does not correspond to s-record file. * ------------------------------------------------------------------------------ * Test HW:         X-MPC5744PE257DC, MPC57xx motherboard * MCU:             PPC5744PFMMM8 1N65H * Fsys:            200 MHz PLL * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * Example configures Sigma_Delta ADC and periodically converts ANA0_SDA0 input * (EVB's potentiometer can be connected i.e. J53-1 --> PO15) and displays * results in the terminal window (USBtoUART bridge J21). Terminal settings is * 19200-8-no parity-1 stop bit-no flow control on eSCI_A. * * ------------------------------------------------------------------------------ * Test HW:         MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU:             PPC5777CMM03 2N45H CTZZS1521A * Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A *                  eSCI_A is USBtoUART bridge (connector J21) * EVB connection:  For ADC: J53-1 (EVB pot's wiper) --> PO15 (header P22) * ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * Application performs basic initialization, initializes interrupts, blinking * one LED by core e200z4a, second by core e200z4b, third by core e200z2, * initializes and display notice via UART terminal and then terminal ECHO. * * ------------------------------------------------------------------------------ * Test HW:         MPC574XG-324DS Rev.A + MPC574XG-MB Rev.C * MCU:             PPC5748GMMN6A 1N81M * Fsys:            160 MHz PLL * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * Terminal:        19200-8-no parity-1 stop bit-no flow control on LINFlexD_2 * ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * This example shows, how to communicate with RTC module PCA8565TS/1 via I2C bus. * For this purpose is used I2C driver created by Petr Stancik. Information from * RTC are sent using DMA via UART. The whole example consists from two parts. * Second part is PC application called GraphicalTerminalExample. This application * handles data from RTC and displays them. RTC also can be set using PC application. * Microcontroller receives data from PC application using DMA via UART. * Received data are written to RTC module. * * UART connection parameters: * Baud rate 19200b/s * 8 data bits * 1 stop bit * none parity * * For correct function of java application, it is required Java 1.8.0_40 * * ------------------------------------------------------------------------------ * Test HW:         MPC5775K-356DS, MPC57xx Motherboard * MCU:             PPC5775KMMY3B 0N76P * Fsys:            PLL0 266MHz *                    Z4 Core 133MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH (debug mode, release mode) * EVB connection: *                     UART connection *                     J14.1 connected to P12.6 (RX) *                     J13.1 connected to P12.7 (TX) * *                     RTC connection *                     RTC pin 4 - connected to any GROUND pin *                     RTC pin 8 - connected to any 3.3V pin *                     RTC pin 6 - connected to P8.10 (SCL - I2C clock) *                     RTC pin 5 - connected to P8.11 (SDA - I2C data) * ********************************************************************************
記事全体を表示