MCUXpresso Secure Provisioning Tool V3.0: failing "Authenticated (HAB)" image build

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCUXpresso Secure Provisioning Tool V3.0: failing "Authenticated (HAB)" image build

跳至解决方案
3,018 次查看
embeddedev
Contributor II

Hello,

I'm trying to build "Authenticated (HAB)" image for MIMXRT1064, using MCUXpresso Secure Provisioning tool version 3.0, but I get following error. I'm using the images for EVK boards
provided by the tool in the data\targets\MIMXRT10##\source_images\ sub-folder. Keys and certificates from "Keys Management" tab are generated ok.

"Unsigned" and "XIP Encrypted (BEE User Keys) Unsigned" images are building fine.

Do you have any idea what could be wrong?


Thank you.

-----------------
elftosb -f imx -V -c "C:\(...)\secure_provisioning21\bd_files\imx_application_gen_win.bd" -o "C:\(...)\secure_provisioning21\bootable_images\evkmimxrt1064_iled_blinky_int_RAM.bin" "D:\(...)\MCUX_Provi_v3\bin\data\targets\MIMXRT1064\source_images\evkmimxrt1064_iled_blinky_int_RAM.s19"
error: line 11: syntax error
Undefined error
Section: 0x14
Section: 0x15
Section: 0x16
Section: 0x18
Section: 0x19
Section: 0x1a
Section: 0x1f
Section: 0x21
error: failed to run code signing tool
elftosb failed
-----------------

0 项奖励
回复
1 解答
3,012 次查看
liborukropec
NXP Employee
NXP Employee

Hello,

 

make sure that the SPT installation and SPT workspace are on the same drive. Either both on C:\ or both on D:\. There's such limitation of windows unfortunately.

 

Regards,

Libor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,013 次查看
liborukropec
NXP Employee
NXP Employee

Hello,

 

make sure that the SPT installation and SPT workspace are on the same drive. Either both on C:\ or both on D:\. There's such limitation of windows unfortunately.

 

Regards,

Libor

0 项奖励
回复
3,010 次查看
embeddedev
Contributor II

Installing on same drive fixed my problem and now all Boot Types are building fine. Thank you! 

0 项奖励
回复