Hello,
I'm trying to build "Authenticated (HAB)" image for MIMXRT1064, using MCUXpresso Secure Provisioning tool version 3.0, but I get following error. I'm using the images for EVK boards
provided by the tool in the data\targets\MIMXRT10##\source_images\ sub-folder. Keys and certificates from "Keys Management" tab are generated ok.
"Unsigned" and "XIP Encrypted (BEE User Keys) Unsigned" images are building fine.
Do you have any idea what could be wrong?
Thank you.
-----------------
elftosb -f imx -V -c "C:\(...)\secure_provisioning21\bd_files\imx_application_gen_win.bd" -o "C:\(...)\secure_provisioning21\bootable_images\evkmimxrt1064_iled_blinky_int_RAM.bin" "D:\(...)\MCUX_Provi_v3\bin\data\targets\MIMXRT1064\source_images\evkmimxrt1064_iled_blinky_int_RAM.s19"
error: line 11: syntax error
Undefined error
Section: 0x14
Section: 0x15
Section: 0x16
Section: 0x18
Section: 0x19
Section: 0x1a
Section: 0x1f
Section: 0x21
error: failed to run code signing tool
elftosb failed
-----------------
解決済! 解決策の投稿を見る。
Hello,
make sure that the SPT installation and SPT workspace are on the same drive. Either both on C:\ or both on D:\. There's such limitation of windows unfortunately.
Regards,
Libor
Hello,
make sure that the SPT installation and SPT workspace are on the same drive. Either both on C:\ or both on D:\. There's such limitation of windows unfortunately.
Regards,
Libor
Installing on same drive fixed my problem and now all Boot Types are building fine. Thank you!