emWin 5.38 User Manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

emWin 5.38 User Manual

ソリューションへジャンプ
2,356件の閲覧回数
saveriomercurio
Contributor II

The emWin library in the MCUXpresso SDK is 5.38, but the NXP web site (emWin Graphics Library|NXP ) only has the manual for 5.30 as the latest for documentation. I've checked on the Segger site, and the current version of the library there is 5.46, and the manual is for that version. There are differences between the 5.30 User Manual and the actual library software. E.g.,, there's a GUI_ANIM_StartEx function in the library, but that function is not in the v5.30 GUI User Manual.

Is the v5.30 User Manual available? If so, can it be placed on the NXP site?

1 解決策
1,668件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Unfortunately Segger doesn't provide user manuals of older versions.

I can provide you the one for version 5.40 (see attachment). With this user manual you can see the release notes on the segger page and just ignore the things that change from version 5.38 to 5.40.

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,668件の閲覧回数
saveriomercurio
Contributor II

Thank you, Victor. 

1,669件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Unfortunately Segger doesn't provide user manuals of older versions.

I can provide you the one for version 5.40 (see attachment). With this user manual you can see the release notes on the segger page and just ignore the things that change from version 5.38 to 5.40.

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信