i have a very simple verilog code to use plu(lpc55s69)
module test(a,b,c);
input a,b;
output c;
assign c=a^b;
endmodule
i click the "Apply verilog configuration" it shows "provide source code fail to compile"
i have tried mcuxpresso ver 11.7,11.8.1, 11.10 etc all have same problem, i tried both verilog text and verilog file. all the same. is there anything need to configured in order to use this function?
thanks.
Hi,
Pls download
As you know that the PLU module is integrated in LPC5569, LPC804 and part of MCXN families, there is a dedicated PLU Config tools, which can generate code to initialize the PLU register based on your logic circuit.
Pls check if you can download the PLU config tools from the website:
https://www.nxp.com/search?keyword=PLU%2520config%2520&start=0
In detail, the PLU Config tools generate code which can initialize PLU registers, you can copy the code to MCUXPresso, compile, it is okay.
Hope it can help you
BR
XiangJun Rong