Is there a demo app for setting up System PLL for the LPCXpresso54608 Board? I could use some legitimate values for the SELR, SELI, SELP, NDEC, MDEC, and PDEC ecoded registers that give me a certain PLL output, also, an explanation for why the encoding/d

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there a demo app for setting up System PLL for the LPCXpresso54608 Board? I could use some legitimate values for the SELR, SELI, SELP, NDEC, MDEC, and PDEC ecoded registers that give me a certain PLL output, also, an explanation for why the encoding/d

1,609 次查看
billclark
Contributor I

Is there a demo app for setting up System PLL for the LPCXpresso54608 Board?  I could use some legitimate values for the SELR, SELI, SELP, NDEC, MDEC, and PDEC ecoded registers that give me a certain PLL output, also, an explanation for why the encoding/decoding of these values is so funky.

0 项奖励
回复
1 回复

1,474 次查看
jeremyzhou
NXP Employee
NXP Employee
Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.
I'd highly recommend you to refer to the driver_examples demos in the SDK, as all demos contain clock configuration part.
You can build the SDK for LPC54608 board via the link below.
Hope this is clear.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复