cannot find -llpc_board_nxp_lpcxpresso_1549

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cannot find -llpc_board_nxp_lpcxpresso_1549

1,132 Views
athmesh_n
Contributor IV

I'm working on Modbus communication, after creating a new project and building gives me the following error

  • c:/nxp/mcuxpressoide_10.2.1_795/ide/tools/bin/../lib/gcc/arm-none-eabi/7.2.1/../../../../arm-none-eabi/bin/ld.exe: cannot find -llpc_board_nxp_lpcxpresso_1549
  • c:/nxp/mcuxpressoide_10.2.1_795/ide/tools/bin/../lib/gcc/arm-none-eabi/7.2.1/../../../../arm-none-eabi/bin/ld.exe: cannot find -llpc_chip_15xx
  • collect2.exe: error: ld returned 1 exit status
  • make: *** [MODBUS_TEST.axf] Error 1

Controller : LPC1517

IDE :   MCUXpresso IDE v10.2.1 [Build 795] [2018-07-25]

Is there any solution ? is there anything to consider before creating the project?

Regards,

Athmesh Nandakumar

Labels (1)
1 Reply

966 Views
converse
Senior Contributor V

It looks like you have created an LPCOpen project (selected during project creation) but either do not have the LPCOpen projects in your workspace, or you have not built them. Note that you need to build LPCOpen in both Debug and Release configurations, so that those equivalent configurations of your project will find the.