Using a PNEV7462 with a 3.3V supply.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using a PNEV7462 with a 3.3V supply.

809 Views
rich3
Contributor II

I am evaluating the PNEV7462. I have successfully compiled and run the example projects using the 5V supply.

I have set the board to the 3.3V supply by switching the JP5 jumper to 3V3. I am now unable to debug the projects.

I am using the LPCLink 2 and MCU Xpresso.

The errors include:

Failed to execute MI command.

Error finishing flash operation.

Target error from Commit Flash write: EP(08). Cannot access cor regs when target running.

GDB protocol problem.

Can you please point me in the right direction?

Thanking you in advance.

Tags (2)
0 Kudos
Reply
1 Reply

749 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

May I ask if you are working with the green board or black board?

Regards,

Ivan.

0 Kudos
Reply