Secure Flash problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Secure Flash problem

跳至解决方案
4,254 次查看
offin
Contributor III

Hello,

Following this topic: https://community.nxp.com/t5/MCUXpresso-IDE/How-to-just-upload-a-binary-file/m-p/1305736 , here is now my new problem.

With
- a KL25 based pcb
- the software MCUXpressoIDE with a KL25 project
- a probe "MCU-link"
- a SWD cable from the pcb to the probe (i shortened it to 10 cm ; see attached picture)
I was able to upload BIN files without problem, until i uploaded a BIN file with secure Flash.
Now each time i execute "Target operation > masse erase" with the script "kinetismasserase.spc", after around 20s (with my oscilloscope, it looks like the probe it trying to communicate with the pcb during this period), there is an error message (see attached screenshot). Then the MCU-link probe is not found anymore even after usb unplug/replug. I have to restart the OS to get the probe visible again.

After the KL25 problem, i tried with
- a KL27 based pcb
- the software MCUXpressoIDE with a KL27 project
- the probe "MCU-link"
- a SWD cable (length 8 cm) from the pcb to the probe
I am able to upload BIN files, and even BIN files with secure Flash. After uploading a BIN file with secure Flash, i execute "Target operation > masse erase" with the script "kinetismasserase.spc", and then the KL27 is unsecure again. So everything works well with the KL27 based pcb.

Another important info
The problem with the KL25 pcb happend already one time some weeks ago. I repeated the "masserase" procedure several times, and i was lucky because after around 20 "masserase" actions, it worked and the Flash has been unsecured. On that time the SWD cable was twice longer. After this problem, i decided to upload only BIN files with unsecure Flash, until i make the mistake again yesterday.

This time, no luck. The KL25 pcb stays desperately locked.

All your tips for new tests will be welcome !

KL25_SDW_cable.jpg

error.png

 

0 项奖励
回复
1 解答
4,201 次查看
ErichStyger
Specialist I

Could you please confirm that, in my situation, without the PEMICRO probe, there is no way to recover the KL25 like it was before

With mass erase disabled, you have locked out yourself from the device. The approach with power cycling using the PEMICRO does not help you in your situation: it helps if the application is doing things out of reset, but not if things are secured by FPROT (this is not 100% true, but would require other expensive equipment as seen on other devices, but I think would go beyond this discussion).

On a side note: if you would have used the SEGGER J-Link, it would have saved you from getting into this situation: the J-Link has two different flash drivers: a 'non-secure' (default) and a 'allow secure' one. with the non-secure it will automatically detect possible dead-end security settings and changes it so you can recover the device (mass-erase enabled).

I hope this helps,

Erich

在原帖中查看解决方案

12 回复数
4,232 次查看
offin
Contributor III

Hi

0 项奖励
回复
4,241 次查看
ErichStyger
Specialist I

looking at your picture with the debug connection, I only see 4 wires but I would expect 5: GND, Vsense, Reset, SWDIO and SWDCLK.

Erich

4,241 次查看
ErichStyger
Specialist I

Of your 'secure' image, what is the security settings? If mass erase is disabled, then you won't be able to regain access to the device (see https://mcuoneclipse.com/2014/06/22/preventing-reverse-engineering-enabling-flash-security/ and https://mcuoneclipse.com/2012/11/04/how-not-to-secure-my-microcontroller/ ).

The other thing you have to consider as possible difference between your two boards is the reset circuit (RESET line) and what you have there (pull-ups, C): The debug probe tries to reset the MCU, and this can fail for several reasons or if you have a pull-up too strong or a C too big this might be difficult. Or if your reset pin has been re-configured or your debug block on the device. What might help you is a faster debug probe (the MCU-Link is good, but not that fast), so you might have better luck with a J-Link or a Multilink. With a Multilink you can try access to the device with power cycling too, see https://mcuoneclipse.com/2021/05/20/recovering-cortex-m-microcontroller-with-a-power-glitch/

 

I hope this helps,

Erich

4,230 次查看
offin
Contributor III

Hi Erich,

Thank you for your answer.
Here are the uploaded data (see attached screenshot)

offin_0-1629048153969.jpeg

After checking.

The interesting byte is EF (0xef = b11101111).
bxxxxxx11 = SECURED
bxxxx1100 = Factory access granted
bxx10xxxx = Mass erase DISABLED
b11xxxxxx = backdoor key access DISABLED

So, yes the mass erase is disabled. Sorry, i did not know it was possible to disable that.
In my opinion, mass erase should be always possible, because it completly erases the Flash so there is no risk of code hack.

0 项奖励
回复
4,204 次查看
ErichStyger
Specialist I

In my opinion, mass erase should be always possible, because it completly erases the Flash so there is no risk of code hack.

You are missing about an important attack vector: with mass erase enabled someone could take over your board/design/product and program it with its own firmware. Depending on your product/company, you very likely don't want this to happen.

I hope this helps,

Erich

4,194 次查看
offin
Contributor III

Yes this is true.
I just thought that microcontrollers products were like computers. I mean no way to avoid such attack vector.

I learn everyday

4,226 次查看
offin
Contributor III

After reading the links above, it looks there can be a chance to unlock the KL25 only with a PEMICRO debug probe, and i unfortunatly do not have this probe.
Could you please confirm that, in my situation, without the PEMICRO probe, there is no way to recover the KL25 like it was before ?

0 项奖励
回复
4,202 次查看
ErichStyger
Specialist I

Could you please confirm that, in my situation, without the PEMICRO probe, there is no way to recover the KL25 like it was before

With mass erase disabled, you have locked out yourself from the device. The approach with power cycling using the PEMICRO does not help you in your situation: it helps if the application is doing things out of reset, but not if things are secured by FPROT (this is not 100% true, but would require other expensive equipment as seen on other devices, but I think would go beyond this discussion).

On a side note: if you would have used the SEGGER J-Link, it would have saved you from getting into this situation: the J-Link has two different flash drivers: a 'non-secure' (default) and a 'allow secure' one. with the non-secure it will automatically detect possible dead-end security settings and changes it so you can recover the device (mass-erase enabled).

I hope this helps,

Erich

4,193 次查看
offin
Contributor III

Thank you for this clear answer.

I give up with this board.
I asked for new KL25 based boards and i will wait for them.
This time i asked for 4 pcs ; this will offer the possibility to make 3 more big mistakes.

I am a beginner in this community. I will click "Accept as solution" in your post. I think this is what i have to do when all is clear and i do not have any other posts to do in this topic. If i have something else to do, please let me know.

Thank you again for your prompt support.

0 项奖励
回复
4,145 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Have you tried the "resurrect" functionality offered by the GUI Flash Tool?

Greetings,
MCUXpresso IDE Support

4,106 次查看
offin
Contributor III

I confirm that the "Resurrect" function does not help. Here is a screenshot of the result.

Capture d’écran du 2021-08-30 11-47-59.png

And after this operation, the software does not find anymore the MCU-Link probe. I have to restart the OS and then it works again.

So i think this pcb is definitely out of order. I am working now with the new fresh arrived ones.

Regarding the "ultimate" secure flash function for future models, i would suggest to setup this in a more complex way. For instance with 16 bits (two bytes of the Flash). Then, unless an unbelievable bad luck, newbies like me could not lock it fortuitously.

0 项奖励
回复
4,139 次查看
offin
Contributor III

Hello,

I remember i tried one or two times the "resurrect" functionality, without success as well.
But i will try again more times.
I am presently out of my office for a couple of days.
As soon as back in office, i will do that and i will post the result.

PS: some extra fresh KL25 pcb's just arrived in my office. This pcb is apparently out of order, but i am safe to work with the new pcb's.

 

0 项奖励
回复