Probes discovered window width or Available attached probes columns width

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Probes discovered window width or Available attached probes columns width

1,050 次查看
piotr_kolodziej
Contributor III

Hello,

I do flashing with "GUI Flash Tool" often with MCUXpresso and I need to select one of several connected boards.

Would it be possible to have any of the following features:

1. Save "Probes discovered" window size or change it's default width in any of the *.xml config files?

2. Save manually changed or automatically calculate "Available attached probes" columns width?

Best regards,

Piotr

标签 (1)
4 回复数

969 次查看
piotr_kolodziej
Contributor III

Hi Erich,

Thx for good news.

Enough would be to know what to enter and in which .metadata\.plugins xml config file.

Best,

Piotr

0 项奖励
回复

968 次查看
ErichStyger
Specialist I

To my understanding, these values are not stored anywhere (for now).

0 项奖励
回复

969 次查看
piotr_kolodziej
Contributor III

I had a hope these values are not stored but perhaps are read if available in config file.
It is OK, only one additional double click before each flashing.

0 项奖励
回复

968 次查看
ErichStyger
Specialist I

Hi Piotr,

if I remember correctly, I had filed a ticket exactly on this. So hopefully this might be implemented in a future release.