FreeRTOS plug-ins have disappeared from my MCXpressoIDE (10.3) on mac.
There is no longer "FreeRTOS" menu on the main bar (File/Edit/Navigate/Search/Project/ConfigTools/Run/Window/Help)
When I go to Window/ShowView/Other there is no any FreeRTOS option.
Is there a way to install freertos TAD back?
In general, I have the feeling that this last version of the IDE is less stable than the previous ones
已解决! 转到解答。
We have managed to replicate this on one machine, but not on several others. We are continuing to investigate, but our current thought is that this is some strange permissions problem.
Can you please try the following and see if this helps?
Make sure the IDE is not running. Then open up a Filer window onto your Applications folder.
Now right click on the "MCUXpressoIDE_10.3.0_2200" directory and select the "Get Info" option.
Open up the "Sharing and Permissions:" entry in the info dialog, and use the "+" button to give the account you are logged in with Read & Write permission.
Then use the wheel drop down and select the "Apply to enclosed items ..." option
Now close the "Get info" dialog, and restart the IDE again.
Do you now see the FreeRTOS menu?
Regards,
MCUXpresso IDE Support
Thanks for confirming that changing the permissions on the install folder got things working for you.
Note that the internal structure of the IDE for v10.3 is very different to the structure used for earlier releases - and the permissions problem is probably something within the install, rather than the top level directory itself. The interesting question that we are still trying to find the answer to though, is why this issue doesn't appear to affect all Macs!
Regards,
MCUXpresso IDE Support
We have managed to replicate this on one machine, but not on several others. We are continuing to investigate, but our current thought is that this is some strange permissions problem.
Can you please try the following and see if this helps?
Make sure the IDE is not running. Then open up a Filer window onto your Applications folder.
Now right click on the "MCUXpressoIDE_10.3.0_2200" directory and select the "Get Info" option.
Open up the "Sharing and Permissions:" entry in the info dialog, and use the "+" button to give the account you are logged in with Read & Write permission.
Then use the wheel drop down and select the "Apply to enclosed items ..." option
Now close the "Get info" dialog, and restart the IDE again.
Do you now see the FreeRTOS menu?
Regards,
MCUXpresso IDE Support
Yes! It's there.
Thank you very much for your support!
PS: Meanwhile I have been using MCUXpresso 10.2.1.0 where I had no problem with the FreeRTOS plugin. The permissions for this 10.2 installation folder are the same that the ones I previously had with 10.3.
Hi Roberto,
whch perspective are you using? The FreeRTOS menu only appears by default in the develop or debug perspective, but not in the normal C/C++ one. So make sure you are in the correct perspective:
I hope this helps,
Erich
Hi Erich,
Thank you very much for your prompt response (and you inspiring work on MCU on Eclipse | Everything on Eclipse, Microcontrollers and Software ).
I am using the "default develop" perspective. I have switched to "debug" and then reset both (dev and debug) perspectives but FreeRTOS is still missing.
Hi Roberto,
thank you :-).
Not sure why the menu does not show up. A few things to check:
Menu Help > Install New software, then click on 'What is already installed', you should have it present here:
is this the case? If not, I have to check other things...
I hope this helps,
Erich
As another data point: that thing had been reported earlier in https://community.nxp.com/thread/481036 . Could you share your workspace metadata\.log file?
Thanks for the log file. It does not show anything interesting for the FreeRTOS plugin.
But it shows:
!ENTRY org.eclipse.equinox.p2.metadata.repository 4 1002 2019-02-01 16:06:49.977
!MESSAGE Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/.
!STACK 0
java.io.IOException: http://freescale.com/lgfiles/updates/Eclipse/ is not a valid repository location.
Have you configured this as a repository? Better you remove/disable it:
But I don't think this is really the cause of your problem.
The other thing I see is that you are starting Eclipse with the -keyring option (which honestly I have never seen/noticed, maybe Mac specific)?
Command-line arguments: -os macosx -ws cocoa -arch x86_64 -keyring /Users/roberto/.eclipse_keyring
What I suggest is to launch Eclipse with the -clean argument: this will re-search for all plugins, and maybe fixes your problem?
As a last resort: you might have to install the IDE again (this is really the last resort). But it would be good if you could keep a copy/backup of your installation, in case anyone from the IDE team has some more ideas what to check or ways to find out what is not working here.
I hope this helps,
Erich
Thank you for your response.
Well, I have downloaded again the MCUXpresso 10.3.0.2200 pkg. After a new install the FreeRTOS tab on the main bar menu is still missing.
What is more, we have tried on another computer from a colleague (mac as well) with the same result (missing FreeRTOS plugin menu).
We are both using MacOS mojave version 10.14.2
PS: I don't know if it might be related but I remember that one day the IDE "lost" the SDK 2.5 installation I have already done (keeping the 2.4.2). I had to install it back.