Headless builds fail with latest mcuxpresso release (11.9.0)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Headless builds fail with latest mcuxpresso release (11.9.0)

856件の閲覧回数
Maarten1
Contributor I

We use a docker image to run headless builds in Bitbucket pipelines.

Up until version 11.7.0_9198 this has been working fine, but with the latest version of the IDE (11.9.0_2144), it stopped working.

The command we are using is:
mcuxpressoide -nosplash -no-indexer --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -build ProjectName/Release -data .

and the error content of the log file is:

 

!ENTRY com.nxp.mcuxpresso.core.datamodels 1 0 2024-01-26 13:58:38.465
!MESSAGE Recreating part support. No part support available.
!SESSION 2024-01-26 13:58:52.354 -----------------------------------------------
eclipse.buildId=unknown
java.version=17.0.7
java.vendor=Eclipse Adoptium
BootLoader constants: OS=linux, ARCH=x86_64, WS=gtk, NL=en_US
Framework arguments:  -no-indexer -application org.eclipse.cdt.managedbuilder.core.headlessbuild -build ProjectName/Release -D BUILD_SERVER_VERSION=1.6.3+73 -D BUILD_SERVER_DATE=26-01-2024 -D BUILD_SERVER_TIME=13:58:28
Command-line arguments:  -os linux -ws gtk -arch x86_64 -no-indexer -application org.eclipse.cdt.managedbuilder.core.headlessbuild -build ProjectName/Release -data . -D BUILD_SERVER_VERSION=1.6.3+73 -D BUILD_SERVER_DATE=26-01-2024 -D BUILD_SERVER_TIME=13:58:28
!ENTRY com.nxp.mcuxpresso.core.datamodels 1 0 2024-01-26 13:58:57.043
!MESSAGE Recreating part support. No part support available.
!ENTRY org.eclipse.cdt.core 4 0 2024-01-26 13:58:57.473
!MESSAGE Error
!STACK 1
org.eclipse.core.runtime.CoreException: description is being loadded
at org.eclipse.cdt.internal.core.settings.model.ExceptionFactory.createCoreException(ExceptionFactory.java:25)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:860)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:817)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$1.run(CExternalSettingsManager.java:431)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager$5.run(CProjectDescriptionManager.java:508)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2382)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runAtomic(CProjectDescriptionManager.java:504)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:472)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:444)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.settingsChanged(CExternalSettingsManager.java:441)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingContainerFactoryWithListener.notifySettingsChange(CExternalSettingContainerFactoryWithListener.java:48)
at org.eclipse.cdt.internal.core.settings.model.CfgExportSettingContainerFactory.handleEvent(CfgExportSettingContainerFactory.java:257)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2190)
at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.fireLoadedEvent(AbstractCProjectDescriptionStorage.java:272)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.getProjectDescription(XmlProjectDescriptionStorage.java:267)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescriptionInternal(CProjectDescriptionManager.java:427)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:409)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:403)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:396)
at org.eclipse.cdt.internal.core.settings.model.CfgExportSettingContainerFactory$CfgRefContainer.getExternalSettings(CfgExportSettingContainerFactory.java:101)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$ContainerDescriptor.getExternalSettings(CExternalSettingsManager.java:163)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.checkExternalSettingsChange(CExternalSettingsManager.java:684)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.processContainerChange(CExternalSettingsManager.java:501)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$2.run(CExternalSettingsManager.java:615)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager$5.run(CProjectDescriptionManager.java:508)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2382)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runAtomic(CProjectDescriptionManager.java:504)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:472)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:444)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.handleEvent(CExternalSettingsManager.java:631)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2190)
at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.fireLoadedEvent(AbstractCProjectDescriptionStorage.java:272)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.getProjectDescription(XmlProjectDescriptionStorage.java:267)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescriptionInternal(CProjectDescriptionManager.java:427)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:409)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:403)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:396)
at com.crt.config.database.TargetConfig.readProjectStorageElement(TargetConfig.java:396)
at com.crt.config.database.TargetConfig.getProjectStorageData(TargetConfig.java:320)
at com.crt.config.database.TargetConfig.getProjectStorage(TargetConfig.java:298)
at com.crt.config.database.TargetConfig.loadTargetConfig(TargetConfig.java:353)
at com.crt.config.database.TargetConfigDatabase.load(TargetConfigDatabase.java:92)
at com.crt.config.database.TargetConfigDatabase.load(TargetConfigDatabase.java:76)
at com.crt.config.database.TargetConfigDatabase.getDefault(TargetConfigDatabase.java:55)
at com.crt.config.database.TargetConfig.findTargetConfig(TargetConfig.java:110)
+ cat /opt/atlassian/pipelines/agent/build/.metadata/.log || true
!SESSION 2024-01-26 13:58:28.524 -----------------------------------------------
eclipse.buildId=unknown
java.version=17.0.7
java.vendor=Eclipse Adoptium
BootLoader constants: OS=linux, ARCH=x86_64, WS=gtk, NL=en_US
Framework arguments:  -no-indexer -application org.eclipse.cdt.managedbuilder.core.headlessbuild -importAll . -cleanBuild lpc15xxLib/Release
Command-line arguments:  -os linux -ws gtk -arch x86_64 -no-indexer -application org.eclipse.cdt.managedbuilder.core.headlessbuild -importAll . -cleanBuild lpc15xxLib/Release -data .
!ENTRY com.nxp.mcuxpresso.core.datamodels 1 0 2024-01-26 13:58:38.465
!MESSAGE Recreating part support. No part support available.
!SESSION 2024-01-26 13:58:52.354 -----------------------------------------------
eclipse.buildId=unknown
java.version=17.0.7
java.vendor=Eclipse Adoptium
BootLoader constants: OS=linux, ARCH=x86_64, WS=gtk, NL=en_US
Framework arguments:  -no-indexer -application org.eclipse.cdt.managedbuilder.core.headlessbuild -build ProjectName/Release -D BUILD_SERVER_VERSION=1.6.3+73 -D BUILD_SERVER_DATE=26-01-2024 -D BUILD_SERVER_TIME=13:58:28
Command-line arguments:  -os linux -ws gtk -arch x86_64 -no-indexer -application org.eclipse.cdt.managedbuilder.core.headlessbuild -build ProjectName/Release -data . -D BUILD_SERVER_VERSION=1.6.3+73 -D BUILD_SERVER_DATE=26-01-2024 -D BUILD_SERVER_TIME=13:58:28
!ENTRY com.nxp.mcuxpresso.core.datamodels 1 0 2024-01-26 13:58:57.043
!MESSAGE Recreating part support. No part support available.
!ENTRY org.eclipse.cdt.core 4 0 2024-01-26 13:58:57.473
!MESSAGE Error
!STACK 1
org.eclipse.core.runtime.CoreException: description is being loadded
at org.eclipse.cdt.internal.core.settings.model.ExceptionFactory.createCoreException(ExceptionFactory.java:25)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:860)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:817)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$1.run(CExternalSettingsManager.java:431)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager$5.run(CProjectDescriptionManager.java:508)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2382)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runAtomic(CProjectDescriptionManager.java:504)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:472)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:444)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.settingsChanged(CExternalSettingsManager.java:441)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingContainerFactoryWithListener.notifySettingsChange(CExternalSettingContainerFactoryWithListener.java:48)
at org.eclipse.cdt.internal.core.settings.model.CfgExportSettingContainerFactory.handleEvent(CfgExportSettingContainerFactory.java:257)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2190)
at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.fireLoadedEvent(AbstractCProjectDescriptionStorage.java:272)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.getProjectDescription(XmlProjectDescriptionStorage.java:267)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescriptionInternal(CProjectDescriptionManager.java:427)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:409)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:403)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:396)
at org.eclipse.cdt.internal.core.settings.model.CfgExportSettingContainerFactory$CfgRefContainer.getExternalSettings(CfgExportSettingContainerFactory.java:101)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$ContainerDescriptor.getExternalSettings(CExternalSettingsManager.java:163)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.checkExternalSettingsChange(CExternalSettingsManager.java:684)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.processContainerChange(CExternalSettingsManager.java:501)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$2.run(CExternalSettingsManager.java:615)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager$5.run(CProjectDescriptionManager.java:508)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2382)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runAtomic(CProjectDescriptionManager.java:504)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:472)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:444)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.handleEvent(CExternalSettingsManager.java:631)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2190)
at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.fireLoadedEvent(AbstractCProjectDescriptionStorage.java:272)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.getProjectDescription(XmlProjectDescriptionStorage.java:267)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescriptionInternal(CProjectDescriptionManager.java:427)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:409)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:403)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:396)
at com.crt.config.database.TargetConfig.readProjectStorageElement(TargetConfig.java:396)
at com.crt.config.database.TargetConfig.getProjectStorageData(TargetConfig.java:320)
at com.crt.config.database.TargetConfig.getProjectStorage(TargetConfig.java:298)
at com.crt.config.database.TargetConfig.loadTargetConfig(TargetConfig.java:353)
at com.crt.config.database.TargetConfigDatabase.load(TargetConfigDatabase.java:92)
at com.crt.config.database.TargetConfigDatabase.load(TargetConfigDatabase.java:76)
at com.crt.config.database.TargetConfigDatabase.getDefault(TargetConfigDatabase.java:55)
at com.crt.config.database.TargetConfig.findTargetConfig(TargetConfig.java:110)
at com.crt.config.database.partssupport.AbstractLinkerScriptHandler.findEntry(AbstractLinkerScriptHandler.java:83)
at com.crt.advproject.custom.optionhandlers.CRPOptionsApplies.getLinkerScriptExtension(CRPOptionsApplies.java:41)
at com.crt.advproject.custom.optionhandlers.CRPOptionsApplies.isOptionValid(CRPOptionsApplies.java:67)
at com.crt.advproject.custom.optionhandlers.CRPOptionsApplies.isOptionVisible(CRPOptionsApplies.java:110)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.setCRPeDefines(CRPOptionsHandler.java:153)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.apply(CRPOptionsHandler.java:52)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.open(CRPOptionsHandler.java:128)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.handleValue(CRPOptionsHandler.java:99)
at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager.performValueHandlerEvent(ManagedBuildManager.java:3093)
at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager.performValueHandlerEvent(ManagedBuildManager.java:3049)
at org.eclipse.cdt.managedbuilder.internal.dataprovider.ConfigurationDataProvider.load(ConfigurationDataProvider.java:406)
at org.eclipse.cdt.managedbuilder.internal.dataprovider.ConfigurationDataProvider.loadConfiguration(ConfigurationDataProvider.java:573)
at org.eclipse.cdt.internal.core.settings.model.CConfigurationDescriptionCache.loadData(CConfigurationDescriptionCache.java:139)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescription.loadDatas(CProjectDescription.java:199)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.loadProjectDescription(XmlProjectDescriptionStorage.java:510)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.getProjectDescription(XmlProjectDescriptionStorage.java:240)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescriptionInternal(CProjectDescriptionManager.java:427)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:409)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:403)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:396)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:636)
at org.eclipse.cdt.core.CCorePlugin.getProjectDescription(CCorePlugin.java:1402)
at org.eclipse.cdt.managedbuilder.internal.core.HeadlessBuilderExternalSettingsProvider.hookExternalSettingsProvider(HeadlessBuilderExternalSettingsProvider.java:63)
at org.eclipse.cdt.managedbuilder.internal.core.HeadlessBuilder.start(HeadlessBuilder.java:661)
at org.eclipse.cdt.managedbuilder.internal.headlessbuilderapp.HeadlessBuilderWrapper.start(HeadlessBuilderWrapper.java:131)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:402)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:77)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:568)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:659)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:596)
at org.eclipse.equinox.launcher.Main.run(Main.java:1467)
at org.eclipse.equinox.launcher.Main.main(Main.java:1440)
!SUBENTRY 1 org.eclipse.cdt.core 4 0 2024-01-26 13:58:57.474
!MESSAGE description is being loadded
!ENTRY org.eclipse.cdt.core 4 0 2024-01-26 13:58:57.475
!MESSAGE description is being loadded
!STACK 1
org.eclipse.core.runtime.CoreException: description is being loadded
at org.eclipse.cdt.internal.core.settings.model.ExceptionFactory.createCoreException(ExceptionFactory.java:25)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:860)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:817)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$1.run(CExternalSettingsManager.java:431)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager$5.run(CProjectDescriptionManager.java:508)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2382)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runAtomic(CProjectDescriptionManager.java:504)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:472)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:444)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.settingsChanged(CExternalSettingsManager.java:441)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingContainerFactoryWithListener.notifySettingsChange(CExternalSettingContainerFactoryWithListener.java:48)
at org.eclipse.cdt.internal.core.settings.model.CfgExportSettingContainerFactory.handleEvent(CfgExportSettingContainerFactory.java:257)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2190)
at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.fireLoadedEvent(AbstractCProjectDescriptionStorage.java:272)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.getProjectDescription(XmlProjectDescriptionStorage.java:267)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescriptionInternal(CProjectDescriptionManager.java:427)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:409)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:403)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:396)
at org.eclipse.cdt.internal.core.settings.model.CfgExportSettingContainerFactory$CfgRefContainer.getExternalSettings(CfgExportSettingContainerFactory.java:101)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$ContainerDescriptor.getExternalSettings(CExternalSettingsManager.java:163)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.checkExternalSettingsChange(CExternalSettingsManager.java:684)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.processContainerChange(CExternalSettingsManager.java:501)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$2.run(CExternalSettingsManager.java:615)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager$5.run(CProjectDescriptionManager.java:508)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2382)
at com.crt.config.database.TargetConfigDatabase.load(TargetConfigDatabase.java:92)
at com.crt.config.database.TargetConfigDatabase.load(TargetConfigDatabase.java:76)
at com.crt.config.database.TargetConfigDatabase.getDefault(TargetConfigDatabase.java:55)
at com.crt.config.database.TargetConfig.findTargetConfig(TargetConfig.java:110)
at com.crt.config.database.partssupport.AbstractLinkerScriptHandler.findEntry(AbstractLinkerScriptHandler.java:83)
at com.crt.advproject.custom.optionhandlers.CRPOptionsApplies.getLinkerScriptExtension(CRPOptionsApplies.java:41)
at com.crt.advproject.custom.optionhandlers.CRPOptionsApplies.isOptionValid(CRPOptionsApplies.java:67)
at com.crt.advproject.custom.optionhandlers.CRPOptionsApplies.isOptionVisible(CRPOptionsApplies.java:110)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.setCRPeDefines(CRPOptionsHandler.java:153)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.apply(CRPOptionsHandler.java:52)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.open(CRPOptionsHandler.java:128)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.handleValue(CRPOptionsHandler.java:99)
at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager.performValueHandlerEvent(ManagedBuildManager.java:3093)
at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager.performValueHandlerEvent(ManagedBuildManager.java:3049)
at org.eclipse.cdt.managedbuilder.internal.dataprovider.ConfigurationDataProvider.load(ConfigurationDataProvider.java:406)
at org.eclipse.cdt.managedbuilder.internal.dataprovider.ConfigurationDataProvider.loadConfiguration(ConfigurationDataProvider.java:573)
at org.eclipse.cdt.internal.core.settings.model.CConfigurationDescriptionCache.loadData(CConfigurationDescriptionCache.java:139)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescription.loadDatas(CProjectDescription.java:199)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.loadProjectDescription(XmlProjectDescriptionStorage.java:510)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.getProjectDescription(XmlProjectDescriptionStorage.java:240)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescriptionInternal(CProjectDescriptionManager.java:427)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:409)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:403)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:396)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:636)
at org.eclipse.cdt.core.CCorePlugin.getProjectDescription(CCorePlugin.java:1402)
at org.eclipse.cdt.managedbuilder.internal.core.HeadlessBuilderExternalSettingsProvider.hookExternalSettingsProvider(HeadlessBuilderExternalSettingsProvider.java:63)
at org.eclipse.cdt.managedbuilder.internal.core.HeadlessBuilder.start(HeadlessBuilder.java:661)
at org.eclipse.cdt.managedbuilder.internal.headlessbuilderapp.HeadlessBuilderWrapper.start(HeadlessBuilderWrapper.java:131)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:402)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:77)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:568)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:659)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:596)
at org.eclipse.equinox.launcher.Main.run(Main.java:1467)
at org.eclipse.equinox.launcher.Main.main(Main.java:1440)
!SUBENTRY 1 org.eclipse.cdt.core 4 0 2024-01-26 13:58:57.474
!MESSAGE description is being loadded
!ENTRY org.eclipse.cdt.core 4 0 2024-01-26 13:58:57.475
!MESSAGE description is being loadded
!STACK 1
org.eclipse.core.runtime.CoreException: description is being loadded
at org.eclipse.cdt.internal.core.settings.model.ExceptionFactory.createCoreException(ExceptionFactory.java:25)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:860)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:817)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$1.run(CExternalSettingsManager.java:431)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager$5.run(CProjectDescriptionManager.java:508)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2382)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runAtomic(CProjectDescriptionManager.java:504)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:472)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:444)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.settingsChanged(CExternalSettingsManager.java:441)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingContainerFactoryWithListener.notifySettingsChange(CExternalSettingContainerFactoryWithListener.java:48)
at org.eclipse.cdt.internal.core.settings.model.CfgExportSettingContainerFactory.handleEvent(CfgExportSettingContainerFactory.java:257)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2190)
at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.fireLoadedEvent(AbstractCProjectDescriptionStorage.java:272)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.getProjectDescription(XmlProjectDescriptionStorage.java:267)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescriptionInternal(CProjectDescriptionManager.java:427)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:409)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:403)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:396)
at org.eclipse.cdt.internal.core.settings.model.CfgExportSettingContainerFactory$CfgRefContainer.getExternalSettings(CfgExportSettingContainerFactory.java:101)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$ContainerDescriptor.getExternalSettings(CExternalSettingsManager.java:163)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.checkExternalSettingsChange(CExternalSettingsManager.java:684)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.processContainerChange(CExternalSettingsManager.java:501)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager$2.run(CExternalSettingsManager.java:615)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager$5.run(CProjectDescriptionManager.java:508)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2382)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runAtomic(CProjectDescriptionManager.java:504)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:472)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.runWspModification(CProjectDescriptionManager.java:444)
at org.eclipse.cdt.internal.core.settings.model.CExternalSettingsManager.handleEvent(CExternalSettingsManager.java:631)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2190)
at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.fireLoadedEvent(AbstractCProjectDescriptionStorage.java:272)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.getProjectDescription(XmlProjectDescriptionStorage.java:267)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescriptionInternal(CProjectDescriptionManager.java:427)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:409)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:403)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:396)
at com.crt.config.database.TargetConfig.readProjectStorageElement(TargetConfig.java:396)
at com.crt.config.database.TargetConfig.getProjectStorageData(TargetConfig.java:320)
at com.crt.config.database.TargetConfig.getProjectStorage(TargetConfig.java:298)
at com.crt.config.database.TargetConfig.loadTargetConfig(TargetConfig.java:353)
at com.crt.config.database.TargetConfigDatabase.load(TargetConfigDatabase.java:92)
at com.crt.config.database.TargetConfigDatabase.load(TargetConfigDatabase.java:76)
at com.crt.config.database.TargetConfigDatabase.getDefault(TargetConfigDatabase.java:55)
at com.crt.config.database.TargetConfig.findTargetConfig(TargetConfig.java:110)
at com.crt.config.database.partssupport.AbstractLinkerScriptHandler.findEntry(AbstractLinkerScriptHandler.java:83)
at com.crt.advproject.custom.optionhandlers.CRPOptionsApplies.getLinkerScriptExtension(CRPOptionsApplies.java:41)
at com.crt.advproject.custom.optionhandlers.CRPOptionsApplies.isOptionValid(CRPOptionsApplies.java:67)
at com.crt.advproject.custom.optionhandlers.CRPOptionsApplies.isOptionVisible(CRPOptionsApplies.java:110)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.setCRPeDefines(CRPOptionsHandler.java:153)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.apply(CRPOptionsHandler.java:52)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.open(CRPOptionsHandler.java:128)
at com.crt.advproject.custom.optionhandlers.CRPOptionsHandler.handleValue(CRPOptionsHandler.java:99)
at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager.performValueHandlerEvent(ManagedBuildManager.java:3093)
at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager.performValueHandlerEvent(ManagedBuildManager.java:3049)
at org.eclipse.cdt.managedbuilder.internal.dataprovider.ConfigurationDataProvider.load(ConfigurationDataProvider.java:406)
at org.eclipse.cdt.managedbuilder.internal.dataprovider.ConfigurationDataProvider.loadConfiguration(ConfigurationDataProvider.java:573)
at org.eclipse.cdt.internal.core.settings.model.CConfigurationDescriptionCache.loadData(CConfigurationDescriptionCache.java:139)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescription.loadDatas(CProjectDescription.java:199)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.loadProjectDescription(XmlProjectDescriptionStorage.java:510)
at org.eclipse.cdt.internal.core.settings.model.xml.XmlProjectDescriptionStorage.getProjectDescription(XmlProjectDescriptionStorage.java:240)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescriptionInternal(CProjectDescriptionManager.java:427)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:409)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:403)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:396)
at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.getProjectDescription(CProjectDescriptionManager.java:636)
at org.eclipse.cdt.core.CCorePlugin.getProjectDescription(CCorePlugin.java:1402)
at org.eclipse.cdt.managedbuilder.internal.core.HeadlessBuilderExternalSettingsProvider.hookExternalSettingsProvider(HeadlessBuilderExternalSettingsProvider.java:63)
at org.eclipse.cdt.managedbuilder.internal.core.HeadlessBuilder.start(HeadlessBuilder.java:661)
at org.eclipse.cdt.managedbuilder.internal.headlessbuilderapp.HeadlessBuilderWrapper.start(HeadlessBuilderWrapper.java:131)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:402)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:77)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:568)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:659)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:596)
at org.eclipse.equinox.launcher.Main.run(Main.java:1467)
at org.eclipse.equinox.launcher.Main.main(Main.java:1440)
!SUBENTRY 1 org.eclipse.cdt.core 4 0 2024-01-26 13:58:57.476
!MESSAGE description is being loadded
 
!ENTRY org.eclipse.osgi 4 0 2024-01-26 13:59:01.423
!MESSAGE Application error
!STACK 1
org.eclipse.swt.SWTError: No more handles [gtk_init_check() failed]
at org.eclipse.swt.SWT.error(SWT.java:4944)
at org.eclipse.swt.widgets.Display.createDisplay(Display.java:1199)
at org.eclipse.swt.widgets.Display.create(Display.java:1123)
at org.eclipse.swt.graphics.Device.<init>(Device.java:167)
at org.eclipse.swt.widgets.Display.<init>(Display.java:632)
at org.eclipse.swt.widgets.Display.<init>(Display.java:623)
at org.eclipse.swt.widgets.Display.getDefault(Display.java:2392)
at org.eclipse.jface.preference.PreferenceConverter.<clinit>(PreferenceConverter.java:100)
at org.eclipse.ui.texteditor.AbstractDecoratedTextEditorPreferenceConstants.initializeDefaultValues(AbstractDecoratedTextEditorPreferenceConstants.java:758)
at org.eclipse.ui.editors.text.TextEditorPreferenceConstants.initializeDefaultValues(TextEditorPreferenceConstants.java:291)
at org.eclipse.ui.internal.editors.text.EditorsPluginPreferenceInitializer.initializeDefaultPreferences(EditorsPluginPreferenceInitializer.java:44)
at org.eclipse.core.internal.preferences.PreferenceServiceRegistryHelper$1.run(PreferenceServiceRegistryHelper.java:307)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.core.internal.preferences.PreferenceServiceRegistryHelper.runInitializer(PreferenceServiceRegistryHelper.java:310)
at org.eclipse.core.internal.preferences.PreferenceServiceRegistryHelper.applyRuntimeDefaults(PreferenceServiceRegistryHelper.java:134)
at org.eclipse.core.internal.preferences.PreferencesService.applyRuntimeDefaults(PreferencesService.java:374)
at org.eclipse.core.internal.preferences.DefaultPreferences.applyRuntimeDefaults(DefaultPreferences.java:225)
at org.eclipse.core.internal.preferences.DefaultPreferences.load(DefaultPreferences.java:279)
at org.eclipse.core.internal.preferences.EclipsePreferences.create(EclipsePreferences.java:371)
at org.eclipse.core.internal.preferences.EclipsePreferences.internalNode(EclipsePreferences.java:624)
at org.eclipse.core.internal.preferences.EclipsePreferences.node(EclipsePreferences.java:759)
at org.eclipse.core.internal.preferences.AbstractScope.getNode(AbstractScope.java:41)
at org.eclipse.core.runtime.preferences.DefaultScope.getNode(DefaultScope.java:77)
at org.eclipse.ui.preferences.ScopedPreferenceStore.getDefaultPreferences(ScopedPreferenceStore.java:222)
at org.eclipse.ui.preferences.ScopedPreferenceStore.getPreferenceNodes(ScopedPreferenceStore.java:251)
at org.eclipse.ui.preferences.ScopedPreferenceStore.contains(ScopedPreferenceStore.java:308)
at org.eclipse.ui.texteditor.ChainedPreferenceStore.getVisibleStore(ChainedPreferenceStore.java:465)
at org.eclipse.ui.texteditor.ChainedPreferenceStore.contains(ChainedPreferenceStore.java:141)
at org.eclipse.xtext.builder.EclipseOutputConfigurationProvider.getBoolean(EclipseOutputConfigurationProvider.java:173)
at org.eclipse.xtext.builder.EclipseOutputConfigurationProvider.createAndOverlayOutputConfiguration(EclipseOutputConfigurationProvider.java:144)
at org.eclipse.xtext.builder.EclipseOutputConfigurationProvider.createAndOverlayOutputConfiguration(EclipseOutputConfigurationProvider.java:153)
at org.eclipse.xtext.builder.EclipseOutputConfigurationProvider.getOutputConfigurations(EclipseOutputConfigurationProvider.java:112)
at org.eclipse.xtext.builder.BuilderParticipant.getOutputConfigurations(BuilderParticipant.java:652)
at org.eclipse.xtext.builder.BuilderParticipant.build(BuilderParticipant.java:247)
at org.eclipse.xtext.builder.impl.RegistryBuilderParticipant$DeferredBuilderParticipant.build(RegistryBuilderParticipant.java:164)
at org.eclipse.xtext.builder.impl.RegistryBuilderParticipant.build(RegistryBuilderParticipant.java:70)
at org.eclipse.xtext.builder.impl.XtextBuilder.doBuild(XtextBuilder.java:525)
at org.eclipse.xtext.builder.impl.XtextBuilder.addInfosFromTaskAndBuild(XtextBuilder.java:455)
at org.eclipse.xtext.builder.impl.XtextBuilder.fullBuild(XtextBuilder.java:562)
at org.eclipse.xtext.builder.impl.XtextBuilder.build(XtextBuilder.java:333)
at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:1020)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:247)
at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:419)
at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:618)
at org.eclipse.core.internal.resources.Project$1.run(Project.java:571)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2382)
at org.eclipse.core.internal.resources.Project.internalBuild(Project.java:609)
at org.eclipse.core.internal.resources.Project.build(Project.java:129)
at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager$2.buildProject(ManagedBuildManager.java:4492)
at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager$2.run(ManagedBuildManager.java:4469)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2382)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2402)
at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager.buildConfigurations(ManagedBuildManager.java:4501)
at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager.buildConfigurations(ManagedBuildManager.java:4381)
at org.eclipse.cdt.managedbuilder.internal.core.HeadlessBuilder.buildConfigurations(HeadlessBuilder.java:324)
at org.eclipse.cdt.managedbuilder.internal.core.HeadlessBuilder.start(HeadlessBuilder.java:724)
at org.eclipse.cdt.managedbuilder.internal.headlessbuilderapp.HeadlessBuilderWrapper.start(HeadlessBuilderWrapper.java:131)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:402)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:77)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:568)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:659)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:596)
at org.eclipse.equinox.launcher.Main.run(Main.java:1467)
at org.eclipse.equinox.launcher.Main.main(Main.java:1440)
0 件の賞賛
返信
4 返答(返信)

764件の閲覧回数
Maarten1
Contributor I

Hi Alice,

thanks for your response.

I have some followup questions regarding your remarks.

1) You say that I need to have an SDK installed. This particular project is using an LPC1518 so as far as I know, there is no SDK involved (nor part support). We also have other projects using processors which do have an SDK, perhaps that works but I haven't tried that yet.

2) I have checked if the GUI runs fine in this docker container, and it does. So no installation issues, there.

3) Same as 1), there is no SDK involved for this project

4) Yeah, I think we don't really need X11 forwarding for the automated buildserver.

As I already mentioned, this same method has been working for years. The only thing that has changed in the environment is the IDE version. If I switch back to the older IDE, everything works. But we really want to have the same version for our developers as for our buildserver. So sticking with the old version is not an option.

That being said, I think that the other discussion you mentioned might have some valuable insights. I will look into that.

 

Kind regards,

Maarten

0 件の賞賛
返信

220件の閲覧回数
otsl
Contributor III
Hey Maarten. I think I'm having the same issue (migrated from 11.4.1 to 11.10.0). If you're still having the issue (or for other people landing here), I believe the issue can be worked around by disabling "Xtext" for the project. See: https://community.nxp.com/t5/MCUXpresso-IDE/Headless-build-fails-for-old-project/m-p/1952136
0 件の賞賛
返信

725件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Maarten1 

Thanks for your sharing and suggestions. 

I will feedback to development team, thanks.

 

BR

Alice

0 件の賞賛
返信

769件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Maarten1 

Thanks for your valuable question.

Our MCUXpresso IDE team give some suggestions as below:

"

1) Quite recently, I’ve done some experiments based on another community report –

see  https://community.nxp.com/t5/MCUXpresso-IDE/Mcuxpressoide-JVM-terminated-Exit-code-1/td-p/1783768 

Command line version of Eclipse works fine but, in that particular case, SDK needed to be installed.

 

2) Regarding the problem described below, first idea would be to make sure the IDE runs correctly with the GUI. So make sure the installer doesn’t throw any kind of error during installation and all dependencies are correctly installed in that Docker container.

 

3) The error “No part support available.“ from the log indicates that the SDK associated to the project being built is not found in the known location (see SDK Handling preferences page, SDK search roots in particular). Either copy it where the IDE expects it to be, either instruct the IDE to use a custom path – search for “change.sdk.roots” in the Release Notes and in the documentation.

 

4)I also see “No more handles [gtk_init_check() failed]” in the log. It’s either caused by the GTK installed on the host, either the IDE is being started without X11 forwarding over SSH.

"

 

Hope it helps.

 

BR

Alice

0 件の賞賛
返信