Changing MCU from 54608 to 54628

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing MCU from 54608 to 54628

1,087件の閲覧回数
anealca
Contributor II

I have imported a project into MCUXpresso v10.

It is for the 54608 MCU but my development board is the 54628.

The code seems to run OK but I would like to change to the correct MCU.

I have both SDK's installed.

When I go to Properties MCU Settings and select the 54628 I get hte warning that the project may not build properly.

This seems to be the case.

The config file (MEX) is not correct (not changed) and the config tool (v5) shows the H/W configuration as the old MCU (54608). I cannot seem to correct this?

What are the correct steps to changing the MCU?

0 件の賞賛
返信
5 返答(返信)

971件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Adrian Neal ,

Right click the error message, then choose  "Switch to processor LPC54628xxx"

as below:

pastedImage_3.png

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

971件の閲覧回数
anealca
Contributor II

Hello @Alice_Yang...

I do not get anything in the problems tab indicating an issue with the MCU.

Only some warnings about var's I've added but have not used...

0 件の賞賛
返信

971件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Adrian,

Please have a look about the Problems view on your attachment :

pastedImage_1.png

BR

Alice

0 件の賞賛
返信

971件の閲覧回数
anealca
Contributor II

Hello @Alice_Yang...

I cannot seem to find this problem anywhere either during compilation or during debugging?

Sad Adrian.

0 件の賞賛
返信

971件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Adran,

Just open the attachment you attached in your original post.

0 件の賞賛
返信