newbie problem. My FRDM-K66F was working before hurricane Irma stole 2 weeks of my time. I downloaded several demo apps I compiled without issue but now the IDE says "no compatible probes available". I did not intentionally change the K20 bootloader firmware from the default openSDAv 2.1 that came loaded by the factory. I am working on a windows 10 laptop and have read that some windows 10 computers may corrupt the bootloader FW in the K20. This may well be operator error!!!
Symptoms:
When I plug in the board to the openSDAv USB port the power LED blinks at about a 1 hz rate forever.
Holding the reset button at power up has no effect.
Pushing the reset button after power up does not affect the board.
The FRDM-K66F debug USB port enumerates as an MBED BOOTLOADER USB Device (as seen in device manager).
No com port appears in device manager.
Background:
I downloaded and ran the following that appeared to work
frdmk66f_demo_apps_hello_world
frdmk66f_demo_apps_bubble
frdmk66f_demo_apps_freertos_hello (could not figure out where to type input text to get to freertos, typing in the IDE console was not echoed and did not appear to do anything.)
I believe the issue may have been coincident with either the freertos_hello app or the frdmk66f_demo_apps_lwip_lwip_udpecho_freertos I tried next.
Questions:
Does the fact the board enumerates as a MBED flash drive mean I have some other (hopefully operator error) issue and not a Win10 corruption issue?
How do I know if the bootloader is corrupt?
If it is K20 corruption do I need to buy a Seeger J-link to recover the bootloader?
I see some old threads discussing this issue. I would prefer to stay on windows 10. Does openSDAv 2.2 fix it? Is it recommended to use if my PC happens to be prone to this issue?
Should windows 10 users "replace the default CMSIS-DAP application with a Segger JLink" FW on the K20 to avoid this?
Also, is there anyway to get the debug console I/O into a putty or terraterm window instead of the IDE?
Is there anyway to talk to a human support engineer to get some help with these startup issues? Sorry, I didn't think so, frustration is setting in.
Thanks,
Tim
(352) 895-3717
已解决! 转到解答。
Hello Tim,
1. Please first try the below :
- Please be sure terminate the other project before debug new project :
Window -> Show View -> Other -> Debug -> Debug
MCUXpresso bug "No debug targets available"
- If still can't work, please delete the .metadata folder under the your MCUXpresso workspace, then reopen MCUXpresso IDE to have a try , use the sample project "frdmk66f_demo_apps_hello_world". If one project can work well, there is no problem with your board.
2. If can't work, you can replace the default CMSIS-DAP application with a Segger JLink or P&E OpenSDA ,
the firmware can find at OpenSDA Serial and Debug Adapter|NXP (If you don't know how to update firmware, let me know .)
3. If still can't work, maybe the bootloader could be corrupted when the board is plugged into a Windows 10 machine.
(As you said there are some project can work well on your board, so in my personal opinion, the bootloader isn't corrupted.)
about the detail please refer to : Freedom OpenSDA Firmware Issues Reported on Windows 10
You can also use other FRDM board program the bootloader, please see the common from Erich on the above thread:
4. "Also, is there anyway to get the debug console I/O into a putty or terraterm window instead of the IDE?"
- When you import the SDK demo, please select as below:
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you Alice.
I was able to recover my debugger connections without buying a seeger J-link probe following your directions. I recorded my steps for posterity and am including it below in case it helps someone else.
Was I supposed to use "03_OpenSDA_FRDM-K66F.bin" FW?
I was able to get the terminal to appear in teraterm, so that worked as well!
Prior to the problem appearing I was able to run programs when I first got the freedom K66F. After the issue surfaced I could not run any programs on the board because I could not get the IDE to talk to the board. When I click the debug icon the build process happens (if needed) and then the probe discovery window pops up and says there no compatible probes available.
I started by opening a debug window in the IDE Window -> Show View -> Other -> Debug -> Debug) and could see a project currently being debugged. The run -> terminate button (and all other upper run -> buttons) was grayed out. I closed the IDE and unplugged the K66F. I reopened the IDE and the debug session was not present. I hit the debug (black bug icon) and got the connect pop up (below) saying no probes avail. The same problem.
I closed the IDE. I deleted the .metadata directory and the hello_world project was no longer shown in the IDE so I could not use it. I deleted the project directory (using windows explorer) and re-imported it. I did not make any other changes. I built the project (successfully) and hit the debug icon (black bug next to red boot) and got the problem pop-up (below).
So, no positive changes so far. I followed the OpenSDA Serial and Debug Adapter|NXP link and saw..
To update your board with OpenSDA applications
Note:
It has been reported that OpenSDA v2/2.1 bootloader could be corrupted when the board is plugged into a Windows 10 machine. For details and more information on resolving this issue, please refer to this community post. Arm Mbed DAPLink bootloaders and applications have been developed on new evaluation boards to address this compatibility issue.
Reprogram your OpenSDA adapter with some new debug, serial, MSD flash-programming application
Select the right debug adapter (Pemicro OpenSDA, Segger JLink or CMSIS-DAP) in your project parameters
On the second bullet (ARM IDE) I hit the link for ARM CMSIS-DAP and was unable to make any sense of that mess. I tried installing the serial driver but it failed. I did the drag and drop from bullet 3, and then un-plug/plug and all is good. My debbuger now connects to the IDE as expected.
Thank you!
Hello Tim,
1. Please first try the below :
- Please be sure terminate the other project before debug new project :
Window -> Show View -> Other -> Debug -> Debug
MCUXpresso bug "No debug targets available"
- If still can't work, please delete the .metadata folder under the your MCUXpresso workspace, then reopen MCUXpresso IDE to have a try , use the sample project "frdmk66f_demo_apps_hello_world". If one project can work well, there is no problem with your board.
2. If can't work, you can replace the default CMSIS-DAP application with a Segger JLink or P&E OpenSDA ,
the firmware can find at OpenSDA Serial and Debug Adapter|NXP (If you don't know how to update firmware, let me know .)
3. If still can't work, maybe the bootloader could be corrupted when the board is plugged into a Windows 10 machine.
(As you said there are some project can work well on your board, so in my personal opinion, the bootloader isn't corrupted.)
about the detail please refer to : Freedom OpenSDA Firmware Issues Reported on Windows 10
You can also use other FRDM board program the bootloader, please see the common from Erich on the above thread:
4. "Also, is there anyway to get the debug console I/O into a putty or terraterm window instead of the IDE?"
- When you import the SDK demo, please select as below:
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------